Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4

Recent discussions

Sort by:
Michael_K
PSoC™ 4
Hello everybody,   I have the following problem: I have two glued boxes which have only 2 free GPIOs and where I have no acceess to the other GPIOs. T... Show More
Joda6568
PSoC™ 4
Hi I want to make an application to get my notifications from an iphone through psoc 4 ble. I'm subscribing to ANCS service, i get the notifications, ... Show More
olto
PSoC™ 4
Hi, Working on a wireless capacitance sensor based on the  CY8C4248LQI-BL583. All components are rated to 85 degC or more. The sensor works fine in ro... Show More
thomasHDSN
PSoC™ 4
Hi, We restart an old project developped with CY8C5568LTI-114 and we want to open the associated project. For the moment, we just want to analyse the ... Show More
JuIn_1625121
PSoC™ 4

CY8C4024FNI-S412(WLCSPパッケージ)の最大リフローサイクル数はいくつでしょうか?

条件などがあれば合わせてご教示いただきたく、よろしくお願いいたします。

liuXQ
PSoC™ 4

使用psoc4000,对设备有低功耗要求,需要对目标识别后延时保持目标,但是延时启动后会增加2ma的功耗,能从哪些方面避免吗

Michl127
PSoC™ 4

Hy, 

how can I set an Interrupt or Reset to wake up the Psoc 4 from deep sleep after aprox 5 minutes? 

mark63122
PSoC™ 4
Hello, Couple questions about the CYBLE-222014-01 BLE module. Pretty much same question as in this post but looking for some clarification: https://community.infineon.com/t5/PSoC-4/CYBLE-222014-01-Bluetooth-5-1/m-p/283316... Show More
MaMi_1205306
PSoC™ 4
Dear Sirs and Madams,   We are considering HSSP for PSoC4. Therefore, I refer to the information of KBA93541.   KBA93541 https://community.infineon.com/t5/Knowledge-Base-Articles/Using-the-CY8CKIT-049-to-Program-Another-PSoC-4-KBA93541/ta-p/257198... Show More
liuXQ
PSoC™ 4
我想使用psoc4000实现15cm左右的接近感应,在超过5cm后SNR很低,想通过ALP_Filter_Library增加SNR,想问一下ALP_Filter_Library需要如何配置和调用。   Show More