Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

lucas_wang
PSoC™ 4
May I ask if there is an MCU that can support IEC 61508? The customer requires a safety integrity level SIL3?Is only Aurix supported? How do I obtain ... Show More
ed234
PSoC™ 4

Is Infineon going to continue production of the PSOC 4200L series of chips? There seems to be a supply issue.

Akshay_Patel
PSoC™ 4
  I first make bin file in PSOC 4. then this file load in android phone and my personal android app. can make possible to load bin file in microcontro... Show More
David_Zhang
PSoC™ 4
hi  infineon:       we know SimpleFOC library is popular  to develop the  BLDC motor ,CY8CKIT-042 is support  Arduino, so  can you develop the SimpleF... Show More
Wilson_Sun8
PSoC™ 4
Dear Sir: We are currently evaluating the RAM&ROM size of CY8C4149AZS-S595(RAM 32KB, Flash 384KB) + FreeRTOSThe result is only using the hello word pr... Show More
songzaiwu
PSoC™ 4
foc
solved msg Solved
  cymc_GFL_math.h              Can you provide the source code? Show More
MiNe_85951
PSoC™ 4
Dear Sirs and Madams,   An offline package was provided in ModusToolbox 3.0, and it was possible to use it completely offline.   I tried to use the ne... Show More
Kurian
PSoC™ 4
Hello, I am trying to measure the pull-down resistor in PSoC-4 by connecting an iDAC to the pin configured as resistive pull-down and measuring the re... Show More
RAM_MARSAKATLA
PSoC™ 4
Dear All, We could not be able to flash our program into CY8C4245AXI-473.Kindly advise on the same Show More
Michael_K
PSoC™ 4
Hello everyone, I have the following problem: My colleague has built a small box with 3 switches for demo purposes. An off and on switch and two switc... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy