PSoC™ 4 Forum Discussions
Hi,
I want to read data from a sensor device over BLE by different clients (smartphones) at the same time. Can this be done with the protocolstack? And if so, are there examples available or is anyone willing to share their code?
Looking forward to your reply,
Kris
Show LessCan I use three PSoC 4 BLEs connected to a single phone at the same time?
I would like to know if this is possible, I have read a bit about the BLE Mesh Network, but I do not know if it can be applied to any PSoC 4, and I still do not understand if the data that is transmitted is the same for each device or each one can send different data.
Show LessHello,
I'm using Capsense and SmartSense to get all the parameters inside my prototype (using the board CY8Ckit-040 with a proximity sensor (pcb)).
I used SmartSense and check the parameters and got for the IDAC modulation and compensation ( 26 and 23) but if I try to use it on a manual mode my raw count is a line and no reaction like a maximum value.
But if I'm using the manual mode and the auto calibration then I got a value at 108 and 92 ( IDAC), all others parameters are the same. And using that value it's working in a manual mode.
Can you explain me why I get a different IDAC with the SmartSense and the manual with auto calibration?
Thank you in advance,
Alex
Show LessHi folks,
I hope you're doing great, I would like to know if someone has been working with PSoC 4 CY8CKIT-042 BLE and NEXTION HMIs, if so can you please tell me what did you do ? I already took a look at the UART APIs datasheet but I didn't figure out how to read the data coming from the HMI and vice versa.
Thanks!
Carlos S.
Show LessFor an agricultural application, I need to design an IoT BT/BLE module operating on a trailer of tractor. The module must communicate wiith a smartphone located in the cabin (distance < 10m). How can I optimize the design for best RF performance? What components will be best suited? What type of antenna would be the best suited?
Thanks for your reply
Kris
Show LessDoes anyone know how to program a CYBLE012011 with miniProg3 via PSoC programmer, asking because I am not able to see my device in the device selection tab? My programmer version is 3.28.1
Show LessI have a project, where I need to communicate 3 PSoC BLE devices simultaneously to a phone. If someone can give me an idea of how to do this, I would really appreciate it.
---------------------
Tengo un proyecto, donde necesito conectar 3 dispositivos PSoC BLE simultaneamente a un teléfono. Si alguien puede darme una idea de como poder realizar esto se lo agradecería mucho.
Show LessI am concerned that CySysFlashWriteRow can write to whatever flash row I hand it.
Is there an API that allows protection when writing to flash, something that will write only to the "free" flash rows in the MCU?
Show Less