PSoC™ 4 Forum Discussions
When the project has 4 buttons,There is no Rsv pin;but 5 buttons,there is;
The project contains 5buttons,How does this Rsv pin connect in PCB ?
Thanks
Magsense 当使用4个buttons的时候没有RSV pin脚,我现在用5个buttons,这个RSV 在PCB 上怎么接呢?
Show Less
Hi,SIR:
Can you please help me solve a problem?
My current customer is using the PS0C4100S series, which has 5 TCPWMs, and the customer expects to generate 5 PWM outputs and needs an additional timer interrupt.
Can a TCPWM module be used as a timer interrupt and PWM output at the same time? If so, how do I set it up? If not, is there any other way to implement timer interrupts?
Thank you for your answer!
Hi,sir,
for PSOC4100S series, is it possible to use GPIO to simulate timer interrupts in addition to the 5-way PWM?
If it is possible, can you provide the example program?
Thanks for the answer!
Show LessDear Sirs and Madams,
We are considering the adoption of the PSoC4 series.
However, it is a condition of adoption that flow implementation is possible.
Reflow profile URL
https://www.cypress.com/file/41231/download
I know there is a Cypress reflow profile, but I have never seen a Cypress flow profile.
Is it possible to provide us with a Cypress flow profile?
Is it deprecated to flow mount a TQFP (0.8mm pitch) package?
Regards、
Show LessHello everyone,
I have a question. Why is there a string of code at the bottom of the chip? How can this happen? Who knows and tells me why???
Look forward to your reply.
Your soon feedback would be appreciated.
Thank you very much.
Best regards,
Qunt Chen
Hi,
I need a USB HID (not CDC !!) bootloader firmware for Psoc4. Does anybody know if such a firmware already exists in cypress universum ?
CDC always needs driver to install. Often user do not like to install driver, so the HID profile is the best solution.
Show LessMy company recently purchased a CY8CKIT-042-BLE Bluetooth® Low Energy (BLE) Pioneer Kit and CY8CKIT-022 CapSense® Liquid Level Sensing Shield in the hope of using them together. We downloaded the PSOC creator and the PSOC programmer and updated the CY8CKIT-042-BLE KitProg firmware.
We then downloaded the Liquid Level Sensing code example from www.cypress.com/CY8CKIT-022. However on attempting to program the device (LLS_CSD_12RX-042.hex) it reported the hex device didn't match the device we wished to program so it couldn't program it.
There are a number of possibilities, I guess.
- Change the device name and recompile the code
- Use a CY8CKIT-042 Kit (without BLE)
I have a CY8CKIT-042, which I can test tomorrow, however I would prefer to use the CY8CKIT-042-BLE kit.
Show LessI may really want to port my PSoC Maker 4.4 activities to ModusToolbox, but it doesn't support the PSoC 4200 family due to the PSoC 4 UDBs, which may be obvious. The PSoC Maker really shows how old it can be and hasn't been updated since October 2020. cps test
Is ModusToolbox expected to fully support the PSoC 4200, and if so, when can we finally expect it?
Show LessHi all,
I'm attempting to enable Miniprog programmer tool Port ID argument handling in my .cli file that I've created. And I will call this .cli using ppcli.exe --runfile.
Example of the my .cli content:
OpenPort MiniProg3/<dynamic port ID here> "C:/Program Files (x86)/Cypress/Programmer/"
As I'm new to PPCLI tool, anyone can advise on this?
Show LessDear Sirs and Madams,
We are considering Host Sourced Serial Programming (HSSP) for PSoC4.
Is it possible to provide us with information about the "TEST_MODE" register (0x40030014)?
I've checked the architecture TRM and the register TRM, but there isn't just a detailed description of this register name (address number).
PSoC4 Architecture TRM URL
Register TRM does not mention anything about this register.
PSoC4 Register TRM
Please let us know if there is any reason not to mention this register.
Regards,
Show Less