Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

odissey1
PSoC™ 4
I cannot use the _setPost to complete operation () API to control the DMA settings. DMA1 is configured to copy the character data array to RAM once, a... Show More
Mungara_07
PSoC™ 4
Hi All     I want to run adxl345 by psoc5 but I can't running in i2c or spi peripheral.     Does anyone have any example code for interfacing a 5LP to... Show More
loop_y0u
PSoC™ 4
Hi Community, I have a CapSense application in which I'm using Interrupt for IR Remote, UART and Touch Interrupt.  The problem I've seen multiple of t... Show More
SenpaiTP
PSoC™ 4
Hello again I have a problem with PSoC Creator not also installing PSoC Programmer on install, even though it happend the first time i installed PSoC ... Show More
jvavra_UICO
PSoC™ 4
Inherited a project using a PSoC4. In the code, I see a "visibility" attribute assigned to some functions, but it's not clear to me what its purpose i... Show More
paddyliu
PSoC™ 4

Dears.

CY8CKIT-145-40XX的CAPSENSE_CSD_Slider_Tuning 实例程序中,打算读取滑条的位置,然后使对应的LED灯点亮,请问有读取滑条位置的代码示例吗?谢谢。

SenpaiTP
PSoC™ 4
Hello Im trying to build a empty project with no components or any code written apart from the autogenerated code. There is a problem with the auto ge... Show More
StephanB
PSoC™ 4
We have an application and a bootloader. In both, the I2C is active. In the application as a master and in the bootloader as a slave. We sporadically ... Show More
Wilton
PSoC™ 4
This was intended to be a supplemental post to the July 18, 2023 post by the same name, but it was locked before I had opportunity to add this.  Since... Show More
GrCa_1363456
PSoC™ 4
Will PSoC 4000T be supported in PSoC Creator? It would be helpful to have all PSoC 4000 devices fully supported with pre-loaded examples and Board Sup... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy