Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

adval22
PSoC™ 4
Hello Infineon Community, I have th CYHVMS-64K-56-001 Evaluation Kit and am looking to get started with it. However, I'm having difficulty finding com... Show More
Abel_W
PSoC™ 4
Hi community,   PSoC Creator 里面似乎只支持头文件直接放在.cydsn 文件夹下面,如果在 .cydsn 文件夹下面再新建文件夹似乎就找不到路径了,请问一下可以添加路径吗?我没有找到可以修改的地方   谢谢 Show More
Abel_W
PSoC™ 4
Hi community,   我在 modustoolbox 里面使用 PSoC4100S MAX 系列的 Demo 板,下载的示例程序,编译的 PDL 文件 cy_gpio.h头文件有 error,虽然有 error 但是还是能够编译成功以及烧录,如下图所示,请问一下怎么解决,谢谢!!!   Show More
MiNe_85951
PSoC™ 4
Dear Sirs and Madams,   We are using PSoC4S MAX to explore configuring a proximity sensor. Is it better to place a mesh ground or an active shield aro... Show More
suno_285741
PSoC™ 4
Hello   I'm using CY8C4745FNI-S412. I want to trim IMO using WCO. But there is no option for trim IMO.   How can I trim IMO using WCO?       Best Re... Show More
DeanG
PSoC™ 4
Hi, I’m using the CY8CKIT-148 (PSoC CY8C4147AZI-S475) and I’m trying to get FW update working without using the DFU library.  I’m mimicking how the mt... Show More
NXTY_Tatebayasi
PSoC™ 4
Hi,  community I was looking at the datasheet and was wondering why the current flowing in Deepl sleep mode for PSoC4000S is 2.5µA(typ) and max 60µA?S... Show More
DeanG
PSoC™ 4
Working with a PSOC4 dev board (CY8KIT-149), trying to get SHA256 and CRC crypto functions working.  Both functions constantly return 0.  Cy_Crypto_En... Show More
georgewangchun
PSoC™ 4
I have created my bootloader and my bootloadable by following the procedure:https://infineon.github.io/dfu/html/index.html#section_dfu_quick_start But... Show More
NiNo_4154496
PSoC™ 4
We are using the PSoC 4.2 BLE chipset and have issues with disconnection. I suspect that the algorithm for detecting and avoiding strong blockers /poo... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy