Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

Sort by:
eremirmak
PSoC™ 4
 We will use  CY8C4247AZA-M483  PArt Number , There will be a lot of cyber-security codes and FUSA algorithms in the products to be designed, I reques... Show More
Bob_G
PSoC™ 4
I am looking for empty carrier tape to be used in the tape-out mechanism of a Xeltek SuperBOT2 automatic programmer.  Does anyone know who at Infineon... Show More
MaMi_1205306
PSoC™ 4
Dear SIrs and Madams,   We are considering configuring the CapSense sensor that connects to PSoC with ITO. ITO seems to have a higher resistance compo... Show More
MaMi_1205306
PSoC™ 4
Dear Sirs and Madams,   We are considering CY8C4247AZS-M483. I searched the website and found the corresponding product.   /* Search result for CY8C42... Show More
divyanshu
PSoC™ 4
Dear Team, We are looking to whitelist the BD-Address for the devices. How can i see the BD-Address of the module from the cypress.? Public address wh... Show More
JoBr_1593366
PSoC™ 4
If I use the I2S component's clip detection, it works fine when USB audio is consuming the data from the I2S component, but if the USB Audio is inacti... Show More
divyanshu
PSoC™ 4
Hi, Am generating the code from an example.If i want to change the variable in the generating source file i can't due to psoc functionality.  I.e I ad... Show More
KaneTW
PSoC™ 4
I'm intending to use a CY8C4724FNI-S402T (due to availability + small package size) part for an application which needs to be powered by a 5V source a... Show More
Lin_Qiang
PSoC™ 4

Hello,

我在使用MiniProg4 操作upgrade Firnware时拔掉USB连接,MiniProg4不能使用了。有什么办法可以恢复吗?

Lin_Qiang
PSoC™ 4
Hello, 当我使用CY8C4146LQS-S423芯片的AD采集功能时,遇到一些问题。当电压值在7V以下时,采集到AD值偏差会很大。 power supply voltage collected voltage 11.9V 11.8V 6.96V 7.2V 6.16V 6.7V... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy