Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

dabo_4430311
PSoC™ 4
Hi everyone, is it fine to call the callback function to increment the timestampgesture only once?I read that I should call it before ProcessWidget an... Show More
dabo_4430311
PSoC™ 4
Hi, relating to the trackpad and pads dimensions, how should I change the Maximum x-axis and y-axis positions?In the CapSense_CSD_P4_Trackpad_Gesture ... Show More
DeCo_1926091
PSoC™ 4
Where can I find a reference document for the C language and libraries used with psoc creator to program PSoC4 ble?Thanks,Dennis Show More
yiar_4652736
PSoC™ 4
Hi,I'm using CapSense Tuner to see 16 sensors on the graph view. However, I can't see the exact value of the sensor signal in the graph. It shows a va... Show More
frro_3974886
PSoC™ 4
On CY8CMBR3116-LQXIT is the pull-up on HI/BUZ/GPO7 mandatory ?When HI/BUZ/GPO7 is used as inetrrupt (Active LOW) is a Floating output when HIGH ?Or th... Show More
KeLa_4479261
PSoC™ 4
Good Evening:I am trying to use the SysTick timer which is part of the cortex M0 family.  I spent some time learning how to use the registers that are... Show More
yiar_4652736
PSoC™ 4
Hi,I currently have CY8CKIT-046 and trying example codes that I found on the Internet. In TopDesign section, I added a second button which has exactly... Show More
YoIs_1298666
PSoC™ 4
Hello,We would like to know about SW_Tx_UART baud rate tolerance.In case of UART(SCB mode)  default oversamping(12) for IMO 24MHz, the tolerance from ... Show More
YuMa_1534086
PSoC™ 4
Hello. Our customer is evaluating CY8C4247LTI-L475.They have questions about software reset. Please confirm and answer below questions. Q1)They used ... Show More
dabo_4430311
PSoC™ 4
I'm trying to use the code example CapSense_Csd_P4_Trackpad_Gestures on a CYBLE_214015_01 (psoc 4 ble), but I keep getting a driver error when connect... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy