PSoC™ 4 Forum Discussions
i has cyble-022001-00 module and i can successfully test hart rate demo application with cysmart mobile app.now i has ONGO payment terminal(hht) and try to scan it but i cant.ONGO device is working as i can pair with it using my android mobile.can any one help?
Show LessHello,
This is a way to enter the LIN slave component in DeepSleep and wake it up from LIN Bus, but It seems that the LIN component is not entered to sleep before executing the CySysPmDeepSleep () API.
In case of PSoC4000S, Is max 55uA of IUART1 in the figure below consumed in addition to the Deep Sleep current consumption?
I wonder if l_ifc_ioctl_LINS (L_IOCTL_SLEEP, NULL) should be executed before executing CySysPmDeepSleep ().
Best regards,
Yocchi
Show Less
Hello Community!,
I Have KitProg2 which is come with this kit
it works well when I'm using it for few weeks. on my office Desktop Computer and as well as in Personal laptop too.
but suddenly it stopped directing in the PSoC programmer Software which is installed on my Laptop. but it still works in my Office Desktop Computer. in both of the machine I have installed the Same PSoC Creator IDE Full. in both machines I'm an Administrator User. KitProg2 Detect in Devices manager of my Laptop but, it's not showing in PSoC programmer See the images. On my Laptop I have reinstalled Whole the PSoC environment (IDE+Programmer). but still, it's not working.
Office Desktop Computer: (Detect in Device manager as well as in PSoC programmer)
My Personal Laptop: (Detect in Device manager But not in PSoC programmer)
Don't know what's the problem.
I hope this can resolve with Community supports.
Thank You 🙂
Show Less
Hello,
We use for a medical device Capsense systems on PSOC4, we constate variation of sensitivity of the system for diferent reason : mechanical, environement, liquids, thikness of treatment on alu, different kind of plastic, coax wiring for transmiting signal ...
For quantify all this system variations and drift in production what is the part of influence of MCU PSOC4 chip-it self? Clocks, IDAC, Compartor, etc...?
What kind of difference we could impute to series of semiconductor batch? Only criteria of sensitivity variation.
Best regards
Show Less
I am trying to use the SPI (SBC mode) with a PSoC 4 MCU and I have the SPI pins displayed and linked to SPI inputs and SPI outputs. I can toggle the SPI pins but as soon as I linked them to the SPI component I cannot control them at all.
Any ideas what am I missing ?
Show LessDear all,
We are looking for an MCU purchase CY8C4245axi-483.
But unable to find it from anywhere.
How can we procure MCU for production?
Thank You.
Show LessHi, I'm developing with a PSoC 4 (CY8C4247AZI-L485) and using among other thinks the USBFS component for USBUART. Sooner or later the Bootloader (via USBFS) will also be used. A very simplified schematic of the project is attached. (VDD caps are missing on purpose.)
My question is what to do with Pin P13.2. There I can't find a definite answer in the documentation. In my layout I have the option to connect VBUS/P13.2 to 5 V from the USB-Bus or the PSoC 5V. Haven't checked in detail, but both options behave very similar. Next on the To-Do list is to disable D+/D- via firmware if VBUS is missing.
Where can I find information how much current is required for VBUS/P13.2 and any recommendation which option is better? Populate R4 or R5?
Show LessHello Everyone,
I do not know how the following code is not working correctly. The thing is that it should be LED should ON regarding into if(CapSense_IsAnyWidgetActive()) statement but code cannot go into if(CapSense_IsAnyWidgetActive()) statement. I checked with LED_Write() function.
"if(CapSense_NOT_BUSY == CapSense_IsBusy()){
CapSense_ProcessAllWidgets();
LED_Write(LED_OFF); " working correctly. I see that LED is turn off but I said before that code cannot go into if(CapSense_IsAnyWidgetActive()) function. How can be possible? What is wrong?
Code:
int main(void)
{
CyGlobalIntEnable; /* Enable global interrupts. */
/* Place your initialization/startup code here (e.g. MyInst_Start()) */
CapSense_Start();
CapSense_ScanAllWidgets();
CapSense_RunTuner();
for(;;)
{
/* Place your application code here. */
if(CapSense_NOT_BUSY == CapSense_IsBusy()){
CapSense_ProcessAllWidgets();
LED_Write(LED_OFF);
if(CapSense_IsAnyWidgetActive()){
LED_Write(LED_ON);
hi
i'm using for training purpose psoc4 kits (CY8CKIT 049-42xx). It works perfectly since laste microsoft win10 update (and works correctly on computer without last microsoft update) but the last update has made the "com" port disappear in the device manager of windows
the cypress kit appears in usb tree but no more in com & lpt port tree
it's ok for usb
but not any more for com & lpt
on computers without windows update i have USB serial port (com5) which appears
I have reinstall the drivers from cypress
https://www.cypress.com/file/135701/download?token=1zfcWWa0
but it does not work
and i don't understand why no warning appears in device manager (everythings seems to be ok but no com port appears)
If someone has a solution it will be good for us - i can't make training practice with my students any more.
Sorry for my english - i'm french and does not speak english usually
thank's
Laurent
Show Less
I think that using the function of BLE in CY8CKIT-042BLE for contact to smart phone. I want to know that how to implement of BLE by PSoC creator. Please teach me the recommended application note, and something else.
Show Less