Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

esill3
PSoC™ 4
I have a PCB using the CY8C4246PVI-DS402 that I am unable to program. In PSoC Creator (Version 4.4.0.80), I can see the MiniProg3, but below that is s... Show More
Sugino
PSoC™ 4
I'm trying to get I2C to work using PSoC Creator, but I'm not getting any signals from I2C.When set to "Strong Drive", I2C works, but when set to "Ope... Show More
loop_y0u
PSoC™ 4
Hi Commmunity,  I'm working on a UART Bootloader Project and trying to find a source like "Bootloader Host" Tool which can Flash the .cyacd file . I o... Show More
BladeCJ
PSoC™ 4
I am trying to use an interrupt to make an LED blink different colors, at different speeds. The target slow frequency is 3 Hz, fast 15 Hz. I am cleari... Show More
HansKlein
PSoC™ 4
Hello, I couldn't find documentation on how to talk to the #HelTec CubeCell LoRa Board w/ the embedded PSoC 4 MCU. Basically, I want to program PSoc... Show More
pv_delfa
PSoC™ 4
Hello together, I am facing some problems with the CY8C4045LQI-S411 IDAC. If I set the range to "RNG_152_4UA" or "RNG_304_8UA" I get the same output r... Show More
Panometric
PSoC™ 4
What are recommended alternatives to CYBLE-012011-00 since it was discontinued?
Harman
PSoC™ 4
Hi, I am working on PSOC 4 (CY8CKIT-041s-MAX PSoC 4100 MAX) I am trying to debug the Non-Blocking Flash Write using Poilling Example project . In this... Show More
npatin_utc
PSoC™ 4
I have a problem when I try to debug a program with a custom board (with a PSoC CY8C4149AZI-S593). It fails with the following messages (especially in... Show More
idream
PSoC™ 4
I only use the MOSI of the SPI to send data, and there is no need for oversampling, how can I increase the rate of the SPI? I See the max baud of SPI ... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy