PSoC™ 4 Forum Discussions
I'm creating a new project using CY8C4125AZI-M433. I have made a couple of clocks and attached them to the clock input of a few components (PWMs, Timers). However, I keep receiving the above error. I don't know what a dsi_out is, the clocks are only going to dedicated component clock inputs. I even tried disabling a few pages to see if I just had too many PWM components, but that didn't seem to help. When I check the resource meter it shows that I'm using 0 digital clocks, I would expect that after adding 2 clocks something would show up there. Am I missing some setup step?
Show LessHi,
I use the CE224899_PSoC4_Low_Power_CapSense_Hybrid_Sensing code demo.
But how do get a long csx button press event ?
Now the situation is that can only get the short press, and then the active state disappears, which function do use to determine the state?
Now is to uses this function -- CapSense_IsWidgetActive(CapSense_BUTTON0_WDGT_ID).
Thanks in advance,
Best regards.
Show Less
Hi,
I am referring to the below examples to test BLE Bonding between two pioneer kits.
Individually the examples work fine. But my requirement is: One pioneer kit should act as a BLE central and will connect to another pioneer kit that is acting as BLE peripheral. BLE peripheral is having below security requirements.
Connection with the peripheral using the Cysmart app works as expected. But how can I tweak the code on central to work with a peripheral with the above GAP settings? Is there an example available for it?
I also have a requirement where I want to restrict the peripheral to be pared/bonded with just one central at a time.
Regards
Show LessHello Team Cypress,
Please recommend a Cypress product that can replace ST-Micro's STM32G0B1KET6N
(STM32G0B1KE - Mainstream Arm Cortex-M0+ 32-bit MCU, up to 512KB Flash, 144KB RAM, 6x USART, timers, ADC, DAC, comm. I/Fs, 1.7-3.6V - STMicroelectronics).
The MCU specifications to be met follow:
-program memory size : 512kB .
-package / case : LQFP-48 ( 7 X 7mm )
-Core : equal or faster than Cortex Arm - M0 core
-interface type : in the needs of UART x4, I2C x1
The client wants to consider Cypress MCU as well if there is a product available that can deliver the features required.
The target MCU will be applied for Transcutaneous electrical nerve stimulation (TENS) therapy device,
The MCU will be used for GPS+LTE controller and will support FOTA update (96Kb).
Is there a Cypress part that meet the specifications above?
If there are parts available and if you could share the Cypress MCU part number, that would be deeply appreciated.
Thank you for your considerations and help to move our business forward.
Sincerely,
Ben
Hi everyone,
When I press button.
I want to read Capsense finger signal value and output to another software .
Which is finger signal in capsense data structure ?
Show Less
Dear Sirs and Madams,
We understand that the CapSense components of PSoC4S are fourth-generation.
The AN85951 CSD(Self) and CSX(Mutual) has been described as up to 200pF as follows.
In addition, the description of the CapSense component datasheet has the following description.
Cp of CSD is up to 61pF.
From the above, both CSD(Self) and CSX(Mutual) does not mean support Cp of up to 200pF, I understand that fourth-generation CSD is up to 61pF and CSX is up to 200pF. Is this recognition correct?
Or does CSD Auto mean up to 61pF and CSD Manual mean up to 200pF?
Regards,
Show LessI am trying to read the voltage of a battery using the SAR ADC but I am not getting the correct values. The ADC outputs 0x7FF0 no matter what the voltage is I am trying to measure. I am using a voltage divider with 357K ohm resistors and an input voltage of 3.8V though this can go as low as 2.5V. The ADC is using an internal Vref of 1.024V. Any help would be appreciated.
Show LessBecause of market availability we remake a board that curretly mount CY8C4245AXI-483 with CY8C4014SXI-420.
But now we cannot program our board with this micro.
Psoc Creator do not find board and psoc programmer try to program with som power cycles but then freeze.
We seen that tring to unsolder some components from board programming goes successfully.
But this solution is not proposable for undreds of board that we have to product.
So, is there a way to program these boards without make hardware modifications ?
We seen some other people have same problem with CY8C4014SXI-421. We tried to program without auto detect, and, try to make a curcuit with transistor on XRES that drive VCC but still don't work.
I attach schematics.
Thanks in advice.
Show Less
Hello,
I have a question about CapSense_SetParam API for PSoC4000S.
If I set "CapSense_BUTTON0_IDAC_MOD0_PARAM_ID" for argument "uint32 paramId", the BAD_PARAM is returned.
Maybe "CapSense_BUTTON0_IDAC_MOD0_PARAM_ID" is not writable.
Is this correct?
What spec says that "CapSense_BUTTON0_IDAC_MOD0_PARAM_ID" is not writable?
Best regards,
Yocchi
Show LessHi
I want to make Eddystone Observer with PSoC4 Devkit.
I was able to read Eddystone TLM & UUID from one beacon device. But I don't know how to associate TLM data and UUID data.
Should I read the advetiser's address?
if its above is correct ,How to read?
I want you to answer my question.
My conddition.
PSoC Creator4.2 BLE componet Ver 4.2
Best regard
Show Less