Announcements

Robots are revolutionizing our lives in many ways. Join our webinar to learn about Infineon’s broad portfolio of robot building blocks.
Click here to register.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

Sort by:
tk1
PSoC™ 4

Please tell me the operating principle of the 5th generation capsense csd.
What are the tuning parameters?

Wilton
PSoC™ 4
I'm working on a design that needs a 25 bit shift register with PLD output taps at 0, 8, 12, 16 and 24. First stage is a D-FF.  But it appears that a ... Show More
Kinrin
PSoC™ 4
Dear guys,   In order to save power, I need to set the MCU into deep sleep mode when there is no working for MCU. I found a API (CySysPmDeepSleep())of... Show More
Pham_Hung
PSoC™ 4
is there any way to do the same with psoc 4 that looks like this image?   Show More
Andreas_Heder
PSoC™ 4
Hello, i have a problem in getting up FreeRTOS for PSoC4: the vTaskDelay(pdMS_TO_TICKS(500)); -> never return MainTask runs only onces.   Main_Task_2... Show More
LYNllow
PSoC™ 4
Hi guys! I'm trying to implement a bootloader where I can reprogram the internal psoc flash with a program stored in an external flash. I'm following this... Show More
MbK
PSoC™ 4
Hello everyone,  I am facing this issue with the CapSense tuner that I cannot seem to troubleshoot.  Is there any solution for this issue. I added scr... Show More
alzh_1341656
PSoC™ 4

BSH 遇到过彩sliver bonding的MCU在damp test中出现migration issue.  作为引进新的part number, 需要确认这个信息。谢谢! 

kirk67
PSoC™ 4

Hi, I need the 3d model for this component: CYBLE-14008-00

 

Many Thanks for Help

kirk67

Kinrin
PSoC™ 4
Dear friends,   I'm trying to build up a program to drive an e-toothbrush. I use 3.7V Li-Ion battery to be the power source. but I found that the ADC ... Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy