Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

GlJe_1688511
Level 4
Level 4
10 likes given 50 questions asked 5 likes given

Hello.

I want to know a operating themperature of CY8C4247LTQ-L485.

Q is Extended Industrial.

pastedImage_0.png

But, a Q temperature of a CY8C4247LTQ-M475 is max 85℃

pastedImage_2.png

Which is the Q temperature a 85℃ or a 105℃?

Do you have the document written it?

Thanks and Best regards.

Glenn.

0 Likes
1 Solution
SampathS_11
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 5 questions asked

Hi Glen,

The Maximum temperature for Q is 105℃. You can find this in the datasheet for CY8C4247LTQ-L485 on the second page, right hand column.

pastedImage_0.png

The datasheet has specifications for both standard and extended industrial parts. Specifications for standard industrial are noted specifically with a maximum temperature of 85℃ in the datasheet, e.g., Table 2 on page 17.

Best regards,

Sampath Selvaraj

View solution in original post

0 Likes
1 Reply
SampathS_11
Moderator
Moderator
Moderator
250 sign-ins 250 solutions authored 5 questions asked

Hi Glen,

The Maximum temperature for Q is 105℃. You can find this in the datasheet for CY8C4247LTQ-L485 on the second page, right hand column.

pastedImage_0.png

The datasheet has specifications for both standard and extended industrial parts. Specifications for standard industrial are noted specifically with a maximum temperature of 85℃ in the datasheet, e.g., Table 2 on page 17.

Best regards,

Sampath Selvaraj

0 Likes