Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4

SlavaB
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Hello,

I created a default DMC project.

SlavaB_0-1624803550585.png

According to the documentation, the resulting hex file should only have one Bootloadable application:

SlavaB_1-1624803629951.png

But in the resulting hex file I see 2 metadata sections and two applications:

SlavaB_2-1624803723096.png

Moreover, these two applications are slightly different. Why?

Regards,
Slava

0 Likes
2 Replies
Alakananda_BG
Moderator
Moderator 250 sign-ins 250 replies posted 100 solutions authored
Moderator

Hi,

Can you share your project with us so that we can verify this at our end.

Can you share the project which uses 4200L kit so that we can debug easily.

Regards

Alakananda
0 Likes
SlavaB
Level 2
10 replies posted 5 replies posted 5 questions asked
Level 2

Hi Alakananda,

I do not think something needs to be debugged. The question was related to compilation phase. I expected a bootable application and received an image with two applications in the hex file.

Regards,
Slava

0 Likes