let me ask you a basic question.
I would like to know the definition of "baseline".
In addition, I would like to know what kind of difference in behavior occurs if I check or uncheck the param 'Enable sensor auto-reset' in Configure CapSense . To do this, I think I first need to know what a Baseline is.
Thank you.
Solved! Go to Solution.
Hi @wangyuanfan
Baseline: The raw count value of a sensor may vary gradually due to changes in the environment such as temperature and humidity. Therefore, the raw count is low-pass filtered to create a new count value known as
the baseline that keeps track of and compensates for the gradual changes in the raw count. The baseline is less sensitive to sudden changes in the raw count caused by a touch. Therefore, the baseline value provides the reference level for computing the signals
Enable Sensor Auto Reset : When enabled, the baseline is always updated. When disabled, the baseline is updated only when the difference between the baseline and raw count is less than the noise threshold.
When enabled, this feature prevents sensors from permanently turning on when the raw count accidentally rises due to a large power supply voltage fluctuation or other spurious conditions.
Because the baseline is always updated when sensor auto reset is enabled, this setting limits the maximum time
duration for which the sensor will be reported as pressed. However, enabling this parameter prevents the sensors from permanently turning on if the raw count suddenly rises without anything touching the sensor. This sudden rise can be caused by a large power supply voltage fluctuation, a high-energy RF noise source, or a very quick temperature change.
Please refer to CapSense design guide - https://www.cypress.com/file/46081/download for more details.
Best regards,
Hari
Hi @wangyuanfan
Baseline: The raw count value of a sensor may vary gradually due to changes in the environment such as temperature and humidity. Therefore, the raw count is low-pass filtered to create a new count value known as
the baseline that keeps track of and compensates for the gradual changes in the raw count. The baseline is less sensitive to sudden changes in the raw count caused by a touch. Therefore, the baseline value provides the reference level for computing the signals
Enable Sensor Auto Reset : When enabled, the baseline is always updated. When disabled, the baseline is updated only when the difference between the baseline and raw count is less than the noise threshold.
When enabled, this feature prevents sensors from permanently turning on when the raw count accidentally rises due to a large power supply voltage fluctuation or other spurious conditions.
Because the baseline is always updated when sensor auto reset is enabled, this setting limits the maximum time
duration for which the sensor will be reported as pressed. However, enabling this parameter prevents the sensors from permanently turning on if the raw count suddenly rises without anything touching the sensor. This sudden rise can be caused by a large power supply voltage fluctuation, a high-energy RF noise source, or a very quick temperature change.
Please refer to CapSense design guide - https://www.cypress.com/file/46081/download for more details.
Best regards,
Hari
I got it ! Thank you so much.