Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello all,

   

I currently have a watchdog timer setup to 2 seconds (divider is 16bit @65535) and would like to extend it to 30 seconds. I use the built in auto generated watchdog timer that uses the LFCLK. Is there any way to do this? Can I use WDT2? If so how??

   

Thanks,

   

Rick

0 Likes
1 Solution
Anonymous
Not applicable

Hello,

   

you can use WDT2, but this 32 bit watchdog timer can´t be used to reset the device, only for interrupts.

   

The second limitation of WDT2 is, that he can only interrupt on a toggle of a single bit from his 32 bits. That means with WDT2 driven by WCO can only interrupt at 16 seconds or 32 seconds, not at 30 seconds.

   

 

   

Another solution is to use a cascade of WDT0 and WDT1. In this case WDT0 acts as 16 bit prescaler for WDT1.

   

This means, if you configure WDT0 to overflow at 65535 ( 2 seconds ), WDT1 counts up by one.

   

You don´t can configure the cascade in Design Wide Resources, you have to use "CySysWdtSetCascade( CY_SYS_WDT_CASCADE_01 );" to configure the cascade of WDT0 and WDT1.

   

Note that WDT0/1 should be disabled before!

   

 

   

For the WDT APIs, you can take a look at "CyLFCLK.c" in the folder "Generted_Source/cy_lfclk" of your PSoC Creator workspace.

View solution in original post

0 Likes
2 Replies
Anonymous
Not applicable

Hello,

   

you can use WDT2, but this 32 bit watchdog timer can´t be used to reset the device, only for interrupts.

   

The second limitation of WDT2 is, that he can only interrupt on a toggle of a single bit from his 32 bits. That means with WDT2 driven by WCO can only interrupt at 16 seconds or 32 seconds, not at 30 seconds.

   

 

   

Another solution is to use a cascade of WDT0 and WDT1. In this case WDT0 acts as 16 bit prescaler for WDT1.

   

This means, if you configure WDT0 to overflow at 65535 ( 2 seconds ), WDT1 counts up by one.

   

You don´t can configure the cascade in Design Wide Resources, you have to use "CySysWdtSetCascade( CY_SYS_WDT_CASCADE_01 );" to configure the cascade of WDT0 and WDT1.

   

Note that WDT0/1 should be disabled before!

   

 

   

For the WDT APIs, you can take a look at "CyLFCLK.c" in the folder "Generted_Source/cy_lfclk" of your PSoC Creator workspace.

0 Likes
Anonymous
Not applicable

Hi Johann,

   

Thank you for your help. I didn't know could use counter 0 as prescaler. That worked out well.

   

Thanks,

   

Rick

0 Likes