Tip / ログイン to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
seaoc_1454951
Level 2
Level 2
10 questions asked 5 replies posted 5 questions asked

PSoC4000Sには32kHzの振動子を接続することによりIMOを±1%にトリミングする機能があります。これをイネーブルにするためにPSoC Creatorにて

・Configure System Clocks -> Low Frequency Clocks TAB 中のWCOにチェックを入れる

・Configure System Clocks -> Hi Frequency Clocks TAB 中のIMOにチェックを入れ、Trim withを WCO を選択

しています。

ユーザプログラムにてWCOを用いてIMO補正する機能が動作していることを確認することが出来るレジスタを教えてください。Low Frequency.jpg

High Frequency.jpg

0 件の賞賛
1 解決策
Anonymous
適用対象外

Aoki-san

本件についてですが、以前Case #00400358にて似たような質問なので、何かご不明な点がればCaseをre-openして、Caseで対応致します。

よろしくお願いいたします。

Nada

元の投稿で解決策を見る

0 件の賞賛
3 返答(返信)
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Dear Aoki-san

Usually the forum language is English. It is a lot of work for everyone who wants to read your questions to translate your posts. It would be much easier when you do that only once for us. So we can easily decide whether we can help you or not.

Regarding your question: Is there any doubt that the trimming of the IMO (which is done in software) does not work, so that you want to controll it?

Regards, Bob

0 件の賞賛
Anonymous
適用対象外

It sounds like he wants to verify the IMO settings by reading the register that contains the IMO trim values/correction from the WCO.

0 件の賞賛
Anonymous
適用対象外

Aoki-san

本件についてですが、以前Case #00400358にて似たような質問なので、何かご不明な点がればCaseをre-openして、Caseで対応致します。

よろしくお願いいたします。

Nada

0 件の賞賛