- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
I would like to used the BLE pa_en functionality on a CYBLE_214015 module to trigger an interrupt.
Is there anyway to achieve this? (See attached project for my attempt)
Regards
Pete
Solved! Go to Solution.
- Labels:
-
PSoC 4 Architecture
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Pete,
The pin P5[0] is not connected for CYBLE214015 module so it is not possible to use pa_en. Please see page no.14 in the BLE component datasheet where it was mentioned that the power amplifier enable (pa_en) output allows you to connect a high active external power amplifier to the device. This output can be routed to the P5[0] digital output pin only.
Thanks,
P Yugandhar.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Pete,
The module CYBLE214015 don't have an integrated Power Amplifier/Low Noise Amplifier to allow for extended communication.
Thanks,
P Yugandhar.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi P
Thanks for responding
I realize the CYBLE214015 doesn't have a PA/LNA or an external connection to P5[0].
As mentioned in the post I don't want to use the pa_en output to drive an external device, I wish to trigger an interrupt from it.
As the attach project shows Ive attempted to connect the pa_en to a pin component to get the interrupt. This doesn't build due to the CYBLE214015 not having the required P5[0] defined, which is the only pin the fitter will assign to pa_en.
However, the schematic for CYBLE214015 shows the PSoC used (CY8C4248FNI-BL593) does have a P5[0], its just not connected to anything. Therefore, it would seem, the restriction to getting this project to build is just the lack of P5[0] being defined/enabled somewhere in the firmware.
Is there some way to add/enable P5[0] to the CYBLE214015 definition?
An alternative option would be to connect pa_en to an internal component, which can generate an interrupt, that the fitter will not attempt to assign to P5[0], ie not a pin. So far I haven't found anything that is compatible with the pa_en output and can get past the fitters requirement to connect pa_en to P5[0].
Regards
Pete
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Pete,
The pin P5[0] is not connected for CYBLE214015 module so it is not possible to use pa_en. Please see page no.14 in the BLE component datasheet where it was mentioned that the power amplifier enable (pa_en) output allows you to connect a high active external power amplifier to the device. This output can be routed to the P5[0] digital output pin only.
Thanks,
P Yugandhar.