- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I've been trying to program the CY8C4245AXI-483 but facing the following error :
Info : http://openocd.org/doc/doxygen/bugs.html
Info : debug_level: 2
Info : adapter speed: 1500 kHz
Info : serial: 101A15C800287400
Info : transport: swd
Info : rst type: soft
Info : adapter speed: 2000 kHz
Info : ** Auto-acquire enabled, use "set PSOC4_USE_ACQUIRE 0" to disable
Info : cortex_m reset_config sysresetreq
Info : none separate
Info : tcl server disabled
Info : Listening on port 4445 for telnet connections
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: JTAG Supported
Info : CMSIS-DAP: FW Version = 2.0.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : KitProg3: FW version: 2.10.878
Info : KitProg3: Pipelined transfers enabled
Info : VTarget = 0.010 V
Info : kitprog3: acquiring PSoC device...
Error: kitprog3: failed to acquire PSoC device
Info : clock speed 2000 kHz
Error: DAP 'psoc4.cpu' initialization failed (check connection, power, etc.)
Error: Failed to connect to the target device
Could you please help me out to solve the programming issue
Solved! Go to Solution.
- Labels:
-
PSoC 4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @saurabh,
Please note that the device CY8C4245AXI-483 belongs to PSoC 4200 family which is not officially supported by Cypress OpenOCD as mentioned in the OpenOCD Readme as shown -
I also noticed that VTarg is detected as 0.01V -
Info : VTarget = 0.010 V
Can you please confirm if the device is powered? Are you using an external supply or is the device powered using MiniProg4?
Also, which tool are you using to connect to the device? Can you please try programming the device using PSoC Creator or PSoC Programmer?
Rakshith M B
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @saurabh,
Please note that the device CY8C4245AXI-483 belongs to PSoC 4200 family which is not officially supported by Cypress OpenOCD as mentioned in the OpenOCD Readme as shown -
I also noticed that VTarg is detected as 0.01V -
Info : VTarget = 0.010 V
Can you please confirm if the device is powered? Are you using an external supply or is the device powered using MiniProg4?
Also, which tool are you using to connect to the device? Can you please try programming the device using PSoC Creator or PSoC Programmer?
Rakshith M B