Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

JaZa_1164481
Level 1
Level 1
First reply posted First like given Welcome!

Is it possible to use the USB debug/upload port of the CY8CKIT 042 development/evaluation  kit (PSoC 4200) in an application without external wires?

I want it to send & receive data through the COMx port in an PC application like the serial send in Arduino but with a shield on its back. Thanks in advance!

1 Reply
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

JaZa,

It is my understanding, that you want to communicate with PSoC4   Pioneer Board using USB-UART bridge, built into PSoC5 programmer. For example, like this

KIT-042_01a_Demo1_A.png

Here PSoC4 UART Tx pin 0.5 is connected to PSoC5  Rx pin 12.6 using an external wire. It is my guess that the wire prevents using an Arduino-style external shield, which you would like to attach on top of the Pioneer Board.

In such case I would recommend to plug the shield, and to solder Tx/Rx wires at the back of the Pioneer Board. For  PSoC4 Tx and Rx pins you need to select any pins that are not used by the shield.

/odissey1

PS. The drawing above was made using free librarie

KIT-042: annotation component for CY8CKIT-042 Pioneer Kit

PSoC Annotation Library v1.0

KIT-042_01a_Default_A.png

0 Likes