Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

RAP_2366941
Level 1
Level 1

I'm using PSOC4 - CY8C4245PVI with external clk of 10Mhz at P0.6. This is working fine.

But my UART (SCB) is not working. I've configure UART for 115200baudrate.

3 Replies
LinglingG_46
Moderator
Moderator
Moderator
1000 replies posted 10 questions asked 5 questions asked

I'm using PSOC4 - CY8C4245PVI with external clk of 10Mhz at P0.6. This is working fine.

How to judge the system work fine?

But my UART (SCB) is not working. I've configure UART for 115200baudrate.

The same project, if you change  HFCLK clock to IMO, does it work?

Could you share your test project here?

0 Likes

How to judge the system work fine?

Driving LED with timer, on/off time of LED is changed according to HFCLK (24Mhz to 10Mhz).

The same project, if you change  HFCLK clock to IMO, does it work?

Yes!!!

0 Likes

1: I use the external clock 4MHz to test the function, the UART can work well.

2: What's the accuracy of the 10MHz? How do you get the clock?

3: Does the voltage match with each other? (PSoC, 10Mhz generator)

4: Choose the right COM Port.

5: Hope it can be helpful for you~

0 Likes