Using Psoc Creator 4.1 and CY84247 module on the CYKit-042. I am using P3.5 as uart tx via SCB1. Everything works fine w the UART, but I need to pull down the TX line for ~1sec to reset comms then turn back to UART TX. How do I reconfigure the P3.5 TX line as a GPIO line and then back to a TX line programmatically at runtime?
Thanks
Wayne
Solved! Go to Solution.
Thanks to e.pratt pointing me in the right direction I found reconfigure thread that has the same requirement as myself. I'm able to successfully;
-Set P3.5 (TX) to GPIO =
//reset required bits to make GPIO, note this changes RX pin to GPIO as well
CY_SET_REG32(CYREG_HSIOM_PORT_SEL3,CY_GET_REG32(CYREG_HSIOM_PORT_SEL3) & 0xFF00FFFF);
//next set desired mode
UART_tx_SetDriveMode(UART_tx_DM_STRONG);
-Drive P3.5 low =
//set drive level as desired
UART_tx_Write(0);
-Set P3.5 to UART TX =
//set required bits to revert GPIO back to UART
//prior to GPIO change CYREG_HSIOM_PORT_SEL3 was 0x00990000 per cyfitter.h
CY_SET_REG32(CYREG_HSIOM_PORT_SEL3,CY_GET_REG32(CYREG_HSIOM_PORT_SEL3) | 0x00990000);
See this thread: Change SWD pins to GPIO at runtime
But, to summarize it here:
"You may set the drive mode of a pin at any time using the appropriate Pin_SetDriveMode() API." @user_1377889
Thanks, the link was not clear to me how to address my issue. I read the UM re Pin_SetDriveMode() and still not understanding how to use this in a practical manner
Pin_1_DM_STRONG Strong Drive
Pin_1_DM_OD_HI Open Drain, Drives High
Pin_1_DM_OD_LO Open Drain, Drives Low
Pin_1_DM_RES_UP Resistive Pull Up
Pin_1_DM_RES_DWN Resistive Pull Down
Pin_1_DM_RES_UPDWN Resistive Pull Up/Down
Pin_1_DM_DIG_HIZ High Impedance Digital
Pin_1_DM_ALG_HIZ High Impedance Analog
I assume the parameter PIN_1_DM_STRONG would actually be PIN_5_STRONG, but how do pass/select the port? Once changed to GPIO how to return the port/pin back to uart?
Can you give a code example;
-Set P3.5 to GPIO
-Drive P3.5 low
-Wait 1sec
-Set P3.5 to UART TX
Thanks for your help
Thanks to e.pratt pointing me in the right direction I found reconfigure thread that has the same requirement as myself. I'm able to successfully;
-Set P3.5 (TX) to GPIO =
//reset required bits to make GPIO, note this changes RX pin to GPIO as well
CY_SET_REG32(CYREG_HSIOM_PORT_SEL3,CY_GET_REG32(CYREG_HSIOM_PORT_SEL3) & 0xFF00FFFF);
//next set desired mode
UART_tx_SetDriveMode(UART_tx_DM_STRONG);
-Drive P3.5 low =
//set drive level as desired
UART_tx_Write(0);
-Set P3.5 to UART TX =
//set required bits to revert GPIO back to UART
//prior to GPIO change CYREG_HSIOM_PORT_SEL3 was 0x00990000 per cyfitter.h
CY_SET_REG32(CYREG_HSIOM_PORT_SEL3,CY_GET_REG32(CYREG_HSIOM_PORT_SEL3) | 0x00990000);