Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

I'm working on a very simple application with logic operators, I assign 3 inputs and 2 outputs, when I build the system it gives message:

Unable to place component "\Comp_0:cy_psoc4_lpcomp_1\". Either the design is bigger than this chip can handle, or the design is over-constrained and there are not enough resources to satisfy the constraints.

I suspect it may be a Psoc creator 3.2 software issue but not 100% sure.

I have chip: CY8CKIT-049-42xx PSOC 4

How can I fix this issue?

1 Solution

In topdesign you need to disable the "System" page, the project needs too many resources.

Bob

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Can you please post your complete project so that we all can have a look at all of your settings. To do so, use

Creator->File->Create Workspace Bundle (minimal)

and attach the resulting file.

Bob

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Here is the complete project:

Thanks

0 Likes

In topdesign you need to disable the "System" page, the project needs too many resources.

Bob

0 Likes