- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello
I am using the internal cock of the CY8C4126AXI-S433, the precision when using the timer has an error, I set a 10 second timer, the timer comes out after 12 seconds. How can I adjust the accuracy? Thank you
Henry
Solved! Go to Solution.
- Labels:
-
PSoC 4 Architecture
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Henry,
What accuracy do you want?
The error ratio of 12 seconds to 10 minutes (600 seconds) is 2%. As described in the datasheet as follows, the maximum error of the IMO internal oscillator is +/-2%.
So, it is not expected to have more accurate internal clock than you experienced.
There is another internal clock ILO and its error is very big as follows.
The maximum error for 10 minutes is -5/+10 minutes.
The PSoC 4100S has Watch Clock Oscillator (WCO) block to generate a LFCLK with a resonator.
It is recommended to add a 32kHz external crystal to have more accurate clock that is available for a timer.
Regards,
Noriaki