Time for save command takes to execute about MBR3

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
hiyac_351831
Level 3
Level 3
25 replies posted 10 replies posted 10 questions asked

Hello,

I find contradiction of "Time of Save command takes to execute" for MBR3 document.

  1. MBR3 datashet

  URL:https://www.cypress.com/file/46236/download

    A sentence "Note 20. Save command takes 220 ms to execute." on p.27 of this datasheet.

    Also, "The time taken to complete the SAVE_CHECK_CRC command is 220 ms typ." on p.32 of this datasheet.

  2. CY8CMBR3xxx Device Programming Specifications

  URL:https://www.cypress.com/file/133376/download

    A sentence "//wait until flash update is complete, max 220 ms" on p.25 of this document.

<Question>

Which is correct for "save command takes 220 ms to execute", typ or max?

Best Regards.

P.S.

I write the same content in Japanese.

---------------------------------------

MBR3についてコマンドの保存にかかる時間は220msと記載されていますが、

この時間はTypかMaxのどちらが正しいでしょうか?

上記に記載しました通り、ドキュメントによって表記が異なっています。

0 Likes
1 Solution
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

I think we should refer to the datasheet, instead of the code explanation.

So I think the 220ms means "typical".

View solution in original post

0 Likes
1 Reply
LinglingG_46
Moderator
Moderator
Moderator
500 solutions authored 1000 replies posted 10 questions asked

I think we should refer to the datasheet, instead of the code explanation.

So I think the 220ms means "typical".

0 Likes