- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi everyone,
I am using the CY8CKIT-042 pioneer kit and PSOC Creator 3.2 SP1 to develop my first PSOC application.
Firstly, I create an example project - BLE HID mouse, after doing the Build and Program, the kit works fine and the Putty on PC can receive the debug message.
And when I create a new project and revise the _write() for using printf() function (refer to the debug.c of example project), when I do the Debug, the firmware will be frozen at printf(), I found it will run into the infinite loop CY_ISR() in Cm0Start.c.
I tried the puts() function, it frozen too; It seems to happen when I called the function of stdio.h.
I have checked the Build Settings of the new project, it is same with the example project.
please see the attached main.c.
Aaron Deng
Solved! Go to Solution.
- Labels:
-
BLE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can you check what is the size of the heap memory allocated to the system from the project's CYDWR -> Systems tab?
Assuming that you have proper libraries to use that function in your system, you may have to increase the memory set for heap size in your project.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Use the sprintf() function, there is no implementation for a system
printer in the libraries.
Regards, Dana.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
but why the example project using the printf() can do ? or I missed something?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can you check what is the size of the heap memory allocated to the system from the project's CYDWR -> Systems tab?
Assuming that you have proper libraries to use that function in your system, you may have to increase the memory set for heap size in your project.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
roit, can you enlighten me about printf() in a psoc project, what is it printing to ?
I do not see any sdtio.h in the workspace after a build, so I cannot figure out what
the STD is ?
Regards, Dana.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Finally, I resolved this problem after growing the heap size to 0x400, the original is only 0x80.
Roit, thanks you very much!!
Does it means that the printf() function will consume more RAM space?
Aaron Deng
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
@Aaron,
Yes, the more heap size allocated, the more RAM will the project consume. If RAM usage is a concern, you can write a loop in your own project to send the data byte by byte over UART and no need to store it in a "file".
@Dana,
The printf() functions internally use character transfer over UART. But before sending, the input is saved as a "file" in the heap and then used to send the character byte by byte. So bigger the "file" that you want to save, the more heap size should be allocated.
Hope this helps.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I dug out this code from a Cypress example:
/* For GCC compiler revise _write() function for printf functionality */
int _write(int file, char *ptr, int len)
{
int i;
file = file;
for (i = 0; i < len; i++)
{
UART_PutByte(*ptr++);
}
return len;
}
This you should provide for using the printf() function directly.
Regarding the heap:
I frequently use malloc() and free() which gets and releases memory from/to the heap instead of using the stack or global data storage. Feels like being quite more flexible. Thus my heap size is usually quite a bit more than 0x0080
Bob