Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Today, while I was studying the problem of npuruss-san,

https://community.cypress.com/thread/37205

I encountered an interesting behavior of SPIS.

With this project I'm using a couple of CY8CKIT-044s,

one for SPI_Master and the other for SPI_Slave.

When I call SPIM_PutArray(), the SPI_Slave receives exact

data assigned by SPIM_PutArray().

But after I call SPIS_PutArray() and when SPI_Master

send another transaction, the MISO data sent out from

SPI_Slave is 1 byte off from the data assigned by SPIS_PutArray().

For example, for the first loop, before SPI_Master sends anything,

I put 0D,0C,0B,0A,09,08,07,06,05,04,03,02,01 to SPIS_PutArray().

When SPI_Master sends commands,  SPI_Slave sends out

00,0D,0C,0B,0A,09,08,07,06,05,04,03,02

(See attached Oscilloscope Screen Shot)

Oscillo_screen.JPG

Naturally, SPI_Master received

00,0D,0C,0B,0A,09,08,07,06,05,04,03,02

although it was expecting to receive

0D,0C,0B,0A,09,08,07,06,05,04,03,02,01.

Then for the next transaction, SPI_Slave prepares sTxBuffer with

F0,E1,D2,C3,B4,A5,96,87,78,69,5A,4B,3C

But SPI_Master receives

01,F0,E1,D2,C3,B4,A5,96,87,78,69,5A,4B

(This 01 seems to be the last byte of the previous PutArray())

Again, SPI_Slave prepare sTxBuffer with

0D,0C,0B,0A,09,08,07,06,05,04,03,02,01

And SPI_Master receives

3C,0D,0C,0B,0A,09,08,07,06,05,04,03,02

(This 3C seems to be the last byte of the previous PutArray())

So I suppose that with this project,

SPIM_PutArray() generates correct data on MOSI pin

but

SPIS_PutArray() generates 1byte data from previous SPIS_PutArray()

before sending the data assigned by current SPIS_PutArray().

Now my question is:

Am I missing something to make SPIS_PutArray() work correctly?

Or is/are there way to reset the data pointer of SPIS

so that I can send correct data?

Attached are my test projects and log/screen copies.

master_log.JPG

slave_log.JPG

moto

0 Likes
1 Solution

Since you are using the SPI Slave component (instead of the SCB SPI component in slave mode), look at the documentation of the _PutArray() method. It says:

If using modes where CPHA = 0, call the SPIS_WriteTxDataZero() function before calling the SPIS_PutArray() function.

The SPIS_WriteTxDataZero() method directly writes into the SPI shift register, which otherwise is pre-occupied with a zero.

View solution in original post

0 Likes
6 Replies
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Without looking at the code: this seems to be expected. When I understand your explanation correctly, your slave just echoes what it received from the master. But only seems to do so after reading one byte.

The master reads data from the slave at the same time it sends out data (or rather: it sends out data with e.g. the falling clock edge, and receives data at the next rising clock edge). So either the slave has data already available as soon as the master starts a transmission, or it can only send it later on.

0 Likes
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Dear user_78878863-san,

Thank you very much for your answer.

But I'm afraid that this is not the case, as from SPI_Slave, tx_buffer is filled by SPIS_PutArray()

way before Master starts the transaction. And it is not echo-ing the data from the SPI_Master.

Currently I am suspecting that there is some mis-implementation in SPIS_PutArray().

But also there is quite a good chance that either the original code or my modification

made some mistake(s) to prevent the function working correctly.

Best Regards,

10-Oct-2018

Motoo Tanaka

0 Likes

Since you are using the SPI Slave component (instead of the SCB SPI component in slave mode), look at the documentation of the _PutArray() method. It says:

If using modes where CPHA = 0, call the SPIS_WriteTxDataZero() function before calling the SPIS_PutArray() function.

The SPIS_WriteTxDataZero() method directly writes into the SPI shift register, which otherwise is pre-occupied with a zero.

0 Likes
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Dear user_78878863-san,

Thank you, you made my day!

I was only referring the API summary and I could not figure out

what SPIS_WriteTxDataZero() was meant for.

Anyway, the program is working perfectly now! (^_^)v

Best Regards,

11-Oct-2018

Motoo Tanaka

0 Likes

Hello,

thank you very much!  It looks like I've made some good progress.

The changes that I made were

1.  use of SPIS_WriteTxDataZero() before each SPIS_PutArray()

2.  reading the "fill" buffers with SPIS_ReadRxData()  (before I did it only when expected meaningful (not fill) data) and this seems to make a lot of difference.

pastedImage_0.png

However I still see some problems on the master side:

Master receives sTxBuffer data from slave in sendCmd().  I expect to receive sFillBuffer data here.  However readStatus() receives sFillBuffer while I expect to receive the sTxBuffer data here.  Also, as you can see bellow, the received data is somehow shifted to the right by one byte.

pastedImage_10.png

What I find interesting is that if I don't use SPIS_WriteTxDataZero() with sFillBuffer then I seem to eliminate the shift problem.

pastedImage_0.png

Another strange thing that I noticed is that master doesn't print "SPI master is running" and "iteration 1" when it starts.

I attached my current updated workspace bundle in the top post of the original discussion(SPI bus: non SCB components ).

Thanks again for your help!

Nikolay Pruss

0 Likes
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Dear Nikolay-san,

In general, "multi post" is supposed to be a bad manner.

And I think the discussion in this thread have been completed.

So let's continue the "egg hunting" at your original thread.

SPI bus: non SCB components

Best Regards,

12-Oct-2018

Motoo Tanaka

0 Likes