cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

Anonymous
Not applicable

 Hi to all,

   

              Can any one suggest me PSoC 4 Specifications to purchase for a laboratory purpose to teach to college students.

   

Thanks and Regards
Rajendra

0 Likes
7 Replies
HeLi_263931
Honored Contributor II

What exactly do you need? There is the PSoC4 technical reference manual (TRM) available at http://www.cypress.com/?rID=78684 and a detailed data sheet at http://www.cypress.com/?rID=78632 . The Pioneet kit documentation is alsow very helpful: http://www.cypress.com/?rID=77780 .

   

Or are you looking for something specific?

0 Likes
Anonymous
Not applicable

 Hi hli,
           nothing in Specific, but it should be generic one.

0 Likes
Anonymous
Not applicable

 Do you want to purchase evaluation boards or just the chip?

0 Likes
Anonymous
Not applicable

 board

0 Likes
ETRO_SSN583
Esteemed Contributor

This board is ~ $ 25, and gives you 2 processors, a PSOC 5LP and a PSOC 4.

   

 

   

You can program PSOC 4 with the 5LP, or program the 4 to do one set of functions,

   

then the 5LP for other advanced capabilties. Cannot beat the price/performance.

   

 

   

    

   

          http://www.cypress.com/?rID=77780

   

 

   

Regards, Dana.

   

 

   

0 Likes
Anonymous
Not applicable

 Agree with Dana

0 Likes
ETRO_SSN583
Esteemed Contributor

Note the board is Arduiono compatible, so you can take advantage

   

of the mass produced low cost shields to plug intop the Pioneer board

   

(shown in my post), like display, SDCARD, Relay, Power Drivers,

   

Zigbee, Wireless, Ethernet......... and board supports PMOD mini

   

boards as well.

   

 

   

0 Likes