Source Current capacity of GPIO of CY8C4147AZI-

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
BiBr_4596811
Level 2
Level 2
5 replies posted 5 questions asked 5 sign-ins

I want to know source current capacity of CY8C4147AZI-S445. For that I have referred this datasheet.

However, Datasheet is of PSoC 4100S Plus family, and I want to know about exact source current capacity of MCU CY8C4147AZI-S445, for confirmation.

Please Help regarding it.

Thank You

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi,

The maximum Source/sink current for the device CY8C4147AZI-S445 is 200 mA. You can find this information in page 17 table 4 of the datasheet.

https://www.cypress.com/file/396611/download

Also, the maximum source current per GPIO pin should be less than or equal to 4mA and maximum sink current per GPIO should be less than 8mA. You can get this information from the pin component datasheet. I have attached the image here.

Please update if you have further queries.

Thanks

Ganesh

View solution in original post

3 Replies
lock attach
Attachments are accessible only for community members.
VenkataD_41
Moderator
Moderator
Moderator
750 replies posted 500 replies posted 250 solutions authored

Hi,

The maximum Source/sink current for the device CY8C4147AZI-S445 is 200 mA. You can find this information in page 17 table 4 of the datasheet.

https://www.cypress.com/file/396611/download

Also, the maximum source current per GPIO pin should be less than or equal to 4mA and maximum sink current per GPIO should be less than 8mA. You can get this information from the pin component datasheet. I have attached the image here.

Please update if you have further queries.

Thanks

Ganesh

cy8c4147 gpio current.jpeg

according to this image from

https://www.cypress.com/file/396611/download

SID4 Maximum current per GPIO is -25mA to +25mA.

Please explain this.

Thank You

Bivay

0 Likes

Hi,

The +/-25mA rating on the device datasheet is absolute maximum ratings which means the pins will get damaged if this level exceeds.

The ratings those are present in the pin component datasheet are limits for proper functional operation. If these limits exceeds the drive logic may be affected.

Thanks

Ganesh