- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
uint8 writeRegister8(uint8 i2c_address, uint8 reg, uint8 data){
if(!I2C_MasterSendStart(i2c_address,0)){
I2C_MasterWriteByte(reg);
I2C_MasterWriteByte(data);
return I2C_MasterSendStop();
}else{
I2C_MasterSendStop();
return 1;
}
}else{
return 99u; //placeholder
}
}
with the loop in my main code being:
for(uint8 i=0; i<BUF_LENGTH; i++){
status = writeRegister8(i2c_address, PWM_REGISTER+i,gamma32[brightness]);
}
I want to replace the loop+function call with I2C_MasterWriteBuf function. However, I2C_MasterWriteBuf does not have a register field. I have tried all sorts of combinations of writing register address first as a byte, restarting the bus, stopping and starting again, writing the buffer directly after setting the register address... Nothing works in terms of that the slave device never gets the right values.
Basic question is: How do I use
I2C_MasterWriteBuf
in an intended way when I need to set a register to write to first?
Solved! Go to Solution.
- Tags:
- psoc4 i2c
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi flhe_4723206,
Instead of having separate variables for register and data, you can have a single structure or single array to hold both these values. You can pass this array/ structure containing both these values as parameter to the I2C_MasterWriteBuf . See attached file for reference.
Let us know if this solves your problem.
Regards,
Bragadeesh
Bragadeesh