Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
odissey1
Level 9
Level 9
First comment on KBA 1000 replies posted 750 replies posted

This is the announcement of the custom component SerialRx v.0.0, implementing simple command line interface between UART Terminal and PSoC microcontroller.

SerialRx: command line UART interface 

Using this component, human-readable UART Terminal messages can be easily received and processed by the microcontroller.

Figure 1. Terminal window showing command messages and PSoC4 responses. Recognized commands ('R_ON') are executed with confirmation echo sent back ('>R_ON'). Unrecognized commands ('foo') are ignored and an error status is reported ('!foo').

SerialRx_P4_SCB_basic_01a_Putty_4.png

 

0 Likes
0 Replies