Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

Hi,
I just received a PSoC 4 unit to evaluate for a potential project/product. I installed creator 2.2 and I have been looking at videos and examples online.

   

I tried creating a simple rs232 comunication test. Receive something from an external source and then append a little string to it and send it back.

   

I must be missing something, bacause I can't get it to work. I assigned TX to P0.5 and RxP0.4.

   

The Rx input pin is set to High Impidance Digital [low(0)]
Tx is set to Resistive pull up. [I tried different options, not sure what to use].

   

I would appreciate any help I could get. Also any information about training resources.

   

The C code looks like this

   

 

   

#include <device.h>

   

void main()
{
    /* Place your initialization/startup code here (e.g. MyInst_Start()) */
    uint8 ch;
   
    UART_1_Start();
    
    UART_1_PutString("Testing RS232 :");
    /* CyGlobalIntEnable; */ /* Uncomment this line to enable global interrupts. */
    for(;;)
    {
        /* Place your application code here. */
        ch = UART_1_GetChar();//UartGetChar();
        //printf("test %c \n",ch);
        if (0u != ch)
        {
        UART_1_PutString("got this ="+ch);
      
        }
    }
}

0 Likes
11 Replies
Anonymous
Not applicable

I forgot to mention that I connected the signal ground (rs232) to pun GND from J3.
[I do not want to set the board as a bridge as it's suggested on the Pioneer kit guide, since the deviced where I plan to use it, doesn't have the USB option. ]

   

For testing I am using a terminal program, and trying to send/receive something. 9600,8,n,1

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

The pioneer kit does not have a RS232 translator on it to get

   

the levels necessary for the physical layer to talk to a PC.

   

Unless you are doing a loopback test at the CMOS interface

   

you cannot get the PC to talk to the UART over RS232.

   

 

   

There are a plethora of RS232 translator chips, and you can always

   

google "RS232 PC Interface" and do it with discretes. Or use a USB

   

to RS232 dongle on PS side.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Hi Dana,

   

Thank you for the reply. Just to be clear.

   

Does this mean I would need a ttl shifter (Like this https://www.sparkfun.com/products/449)

   

In the past I have used a MAXIM 232cpe, would either of this two options work for me? 

   

Also what would be the maximum number of UARTs [rs232] that I should be able to defined? [I think I read that PSoC 4 had 2 UARTs] can I only define 2 or can the board "play some trics" to expand that number? 

   

 

   

Thank you so much for your help,

   

 

   

Cristian

0 Likes
Anonymous
Not applicable
        Hi, Something for you.   
1) Permit global interrupt, user module might be use it.   
2) I think, Tx pin might be Strong drive and initial value is high,   
It would be better.   
3) What is this? [ UART_1_PutString("got this ="+ch); ]   
This is a C language, not have string class as C++   
0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Maxim 232 excellent choice.

   

 

   

As far as max UARTs, take a look at the software UART and its API sizes.

   

Uses no UDB resources.

   

 

   

Regards, Dana.

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

 UART_1_PutString("got this ="+ch);

   

is correct C, but does not do what you expect,

   

Use two statements, one to send the fixed text as a string and one to send the character as a byte.

   

 

   

Bob

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

There are some UDBs within the PSoC4 which can be used to build additional hardware. Try to implement one or two UART modules, connect the pins (Needed to prevent the UARTs from getting optimized-out) and see if the project fits, I did not try that yet.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thank you for your comments. I added a MAX232xxx and I had communication two ways after that. The buffer seemed to be limited to 4bytes. I tried to just change the component (UART) buffer size, but that seems to requiere the use of interrupts.

   

Are there any examples of the use/implementation of this interrupts? or use larger string messages?

   

Thank you for your help,

   

 

   

Cristian

0 Likes
Anonymous
Not applicable

I normally use a ring buffer for RX and own interrupt RX routine. 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

When extending the buffer to more than 4 bytes will start an INTERNAL interrupt procedure, so there is no need (except for enabling global interrupts) for you to act.

   

The routines are blocking, so there is no need to increase the buffer. The routine will return when all bytes are sent.

   

HL applied for a different approach we always suggest here since it is a VERY good exercise and is rather helpful:

   

Write an interrupt driven routine that accepts characters from UART in a (so called) circular buffer.

   

Same (or similar) for ta circular buffer from which characters are fetched an transferred via UART.

   

 

   

 

   

Bob

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

3) What is this? [ UART_1_PutString("got this ="+ch); ]

   

 

   

You cannot concatenate strings or other to a string this way in C.

   

Convert the numeric to a string, then use

   

 

   

char *cstrcat(char *dest, const char *src); in the extended

   

library to concatenate the strings. Don't forget to size the receiving

   

string array to total length expected + 1 for nul termination character.

   

 

   

Regards, Dana.

0 Likes