Psoc 4000S MCU CY8C4025FNI-S402T programming

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
deonc_3697476
Level 2
Level 2
First like given

From the Psoc 4000S family datasheet it says the chips can be programmed from a SWD interface. I am including an SWD interface in my PCB design for the CY8C4025FNI-S402T chip, but I was wondering whether the chip supports programming via UART or SPI as well.

I know the Segger J-Link JTAG/SWD device can be used to program or debug over SWD, but will the Cypress KitProg device also be able to connect into the SWD interface in a PCB to program a CY8C4025FNI-S402T chip soldered onto the PCB? Thanks!

0 Likes
1 Solution
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

Hi,

You can do bootloading to update the  product’s firmware over UART or I2C, please check these following ANs for  details :

http://www.cypress.com/file/45171/download

http://www.cypress.com/documentation/application-notes/an86526-psoc-4-i2c-bootloader

You can use kitprog to program CY8C4025FNI-S402 ( WLCSP package ) chip, CY8CKIT-059 is available with snap-away Programmer and Debugger (Kitprog) on the USB connector whose details are available at this link:

http://www.cypress.com/documentation/development-kitsboards/cy8ckit-059-psoc-5lp-prototyping-kit-onb...

View solution in original post

0 Likes
1 Reply
AnkitaS_51
Employee
Employee
100 likes received 50 likes received 25 likes received

Hi,

You can do bootloading to update the  product’s firmware over UART or I2C, please check these following ANs for  details :

http://www.cypress.com/file/45171/download

http://www.cypress.com/documentation/application-notes/an86526-psoc-4-i2c-bootloader

You can use kitprog to program CY8C4025FNI-S402 ( WLCSP package ) chip, CY8CKIT-059 is available with snap-away Programmer and Debugger (Kitprog) on the USB connector whose details are available at this link:

http://www.cypress.com/documentation/development-kitsboards/cy8ckit-059-psoc-5lp-prototyping-kit-onb...

0 Likes