Hello,
I have a similar problem to this:
I want to exchange the keyboard shortcuts build.build project (Shift+F6) and build.build workspace (F6).
I cannot remove the shortcuts or assign them to the other function.
I can assign other combinations which are not taken already but i cannot remove them again.
I get the same error message as shown in the link above - "Sorry but the key 'xyz' is protected and cannot be assigned or removed.
I did this on a different pc and it worked. On both PC I recently installed PSoC Creator 4.4.
The only difference I see is that on the PC where it does not work, PSoC Creator 4.2 was previously used, whereas the PC where it worked was freshly set up.
I hope for a quick solution as I need to remove the nonsensical combination I added as a test xD
Solved! Go to Solution.
Well, I opened a project and tried again to remove/reassign the shortcuts and it worked.
It's a mystery to me why this won't work when no project is open but I guess this thread may be closed now.
Well, I opened a project and tried again to remove/reassign the shortcuts and it worked.
It's a mystery to me why this won't work when no project is open but I guess this thread may be closed now.