Attachments are accessible only for community members.
Anonymous
Not applicable
Dec 22, 2015
05:00 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Dec 22, 2015
05:00 AM
I started with the Low Power CapSense project with tuning. I have a custom CapSense board that I'm trying to run with the two wakeup modes in that project. If there is no touch, put the micro into deep sleep, wake up every ~100 ms to scan the prox sensor, if you get a touch wake up ,scan every ~30ms to update the touch positions. The problem is the board doesn't seem to wake up with the prox. sensor.
It depends on this function, proximityState = CapSense_CheckIsWidgetActive(CapSense_PROXIMITYSENSOR0__PROX);
returning a 1 when it sees a touch, but this is always 0.
Any ideas? I'm wondering if I set up the Proximity Sensor right in the configuration.
1 Reply