Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello,

   

I am trying to program the CY8C4013sxi-400 chip with SOIC 8 pin package using
Kit Prog of Cypress PSoC5LP Prototype Kit: CY8CKIT-059
http://www.cypress.com/documentation/development-kitsboards/cy8ckit-059-psoc-5lp-prototyping-kit

   

The CY8C4013SXI-400 belongs to the PSoC4000 family and uses power cycling to enter Debug.

   

 

   

Here are the connections

   

KitProg VTARG => VDD Pin 4

   

KitProg GND => VSS Pin 5

   

==> VCCD Pin 3 ---- 0.1uF to GND

   

KitProg SWDIO => Pin8

   

KitProg SWCLK => Pin1

   

 

   

The PSoC programmer is unable to detect the Microcontroller with this.
I would like to know what would be the best way to get this chip programmed.

   

Thanking in Advance,

   

Regards,
Bose

0 Likes
6 Replies
Anonymous
Not applicable

Hello,

   

I have checked both these documents.
But, they only talk about the power cycling as measure for replacement of XRES.

   

However Kitprog does not have power cycling, so I additionally implemented this in the circuit bu having physical disconnection available on the board. But still this did not work.

   

I am looking for an exact solution for the programming of the CY8C4013sxi-400 chips.

   

Kindly help me out.

   

Regards,
Bose

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Consider filing a CASE on this -

   

 

   

To create a technical or issue case at Cypress -

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Thanks,

   

I will try that out.

0 Likes
Anonymous
Not applicable

Hi Bose,

   

I've the same problem with the SO8 devices. May you please give me a feedback, when you receive a qualified answer!

   

tectoy

0 Likes

I have been able to program them using the kitprog and PSOC programmer, a pain though, it will not work in PSoC creator, nor will it enter debug.

The voltage has to be at 3.3V, will not work at 5V.

0 Likes