- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am using CYBLE-212020-01 modules which sends and receives some values over BLE from App.
I use Over-the -Air (OTA) firmware update.
The workspace encloses three projects functions are as follows:
1. Launcher project
The purpose of the project is to:
- Start either the Stack or Application project image
- Copy the Stack project image from a temporary location to the persistent location (just after the Launcher project image).
2. Stack project (contains the BLE Stack)
The purpose of the project is to:
- Host the BLE Stack
- Upgrade the Application project image
- Upgrade the Stack project image itself
- Receive updates for the Stack project image itself or for the Application project image
3. Custom Apllication Project
The Stack project is the bootloader.
The problem raise when I update firmware only with wrong apllication build with a different stack. After the update the firmware is lock in the launcher project and I can't put the system in bootloader state. How I can fix this? How I put the firmware in bootloader state when the application is wrong in order to correctly update the correct application and the correct stack?
Thanks in advance for any replies.
Lucia
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Stack application and user application images are upgradable over BLE. Whereas, launcher project is not upgradable. Please note that to update launcher project, user needs to perform programming.
User application project uses BLE stack from stack project. So, user needs to update both stack and user application images after updating BLE component. In your case, which are the components updated in the stack and user application projects?
Bootloader performs validation of next project to be loaded. It seems that validation fails at your end. You can refer to section: ‘Launcher/Combined Application Project Functions’ in bootloader component datasheet to understand the flow. I tried to upgrade all components in Upgradable stack OTA code example projects (launcher, stack and user application) in PSoC Creator 4.2 including BLE. Bootloading the user application bootloading fails at my end. Whereas, if I upgrade all components except BLE, the user application upgrade is successful and control is passed to user application project.