I'm using PSoC Creator 3.3. and Psoc4-042. Working on the BLE project with led blinking. I'm facing error from the clock and PWM at the 100Hz frequency. The error window is attached in the files. Please kindly look after.
This error is not only is this program, I'm facing this error in every program i was doing at 100Hz Hardware handling.
Thank you
Br- Gaurav Badgujar
Solved! Go to Solution.
Changed clock to 1kHz
changed PWM width to 16 bits
changed PWM period to 999 (1 second)
changed compare value to 499
changed main() to start the PWM
Bob
Welcome in the forum, Gaurav!
The cause of the error is listed in the first line of your compiler output. The clock divider is 16 bit wide. Hence the max divisor is 65536. From your HFCLK of 48MHz you would need a divider of 480,000.
Workaround: Change the PWM period and compare values to 10 times higher and use a 1kHz input clock.
Bob
Thanks, Bob
please guide me for 1Hz PWM output.
what will be the Period value and Compare value and the clock i/p?
Best would be to post your complete project, so that we all can have a look at all of your settings. To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.
Furthermore a bit of explanation what you want to perform with your project (apart from blinking an LED at 1 Hz) could give you some more hints.
Bob
It is working for me.
thank you, Bob.