cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

MaMi_1205306
Honored Contributor

Hi,

I will discuss the contents of the past inquiries once again.

I have heard that the behavior in question has been reproduced.
Have you found this problem?

PSoC4S CY8C4126AXI-S445 EXTCLK settings

As we confirmed, even PSoC4 does not work depending on the series.

PSoC4S has confirmed the operation of changing clock.
However, it does not work with PSoC4S +.

PSoC4S : CY8CKIT-145

PSoC4S+ : CY8CKIT-149

Both of them have the same project contents and input the external clock to P0[6].

Is there any necessary steps to switch clocks?

Regards,

0 Likes
1 Solution
Ekta
Moderator
Moderator

Hello Masashi,

Please use the following code for switching clock to EXTCLK in case of PSoC 4100S Plus

#include "project.h"

int main(void)

{

    CY_SET_REG32((void *)(CYREG_HSIOM_PORT_SEL0), (CYVAL_HSIOM_IO0_SEL_ACT_0 << (6 * 4))); /* HSIOM_IO0_SEL_ACT_0 */

    CY_SET_REG32((void *)(CYREG_GPIO_PRT0_PC), (LED_DM_DIG_HIZ << (6 * 3))); /* High Impedance Digital */

    /* 6 is a pin number, 3 and 4 are bitfield widths */

    CySysClkWriteHfclkDirect(CY_SYS_CLK_HFCLK_EXTCLK);

    for(;;)

    {

        LED_Write(0);

        CyDelay(500);

        LED_Write(1);

        CyDelay(500);

    }

}

I have attached the sample project below.

Best Regards

Ekta

View solution in original post

0 Likes
4 Replies
Ekta
Moderator
Moderator

Hello Masashi,

Please use the following code for switching clock to EXTCLK in case of PSoC 4100S Plus

#include "project.h"

int main(void)

{

    CY_SET_REG32((void *)(CYREG_HSIOM_PORT_SEL0), (CYVAL_HSIOM_IO0_SEL_ACT_0 << (6 * 4))); /* HSIOM_IO0_SEL_ACT_0 */

    CY_SET_REG32((void *)(CYREG_GPIO_PRT0_PC), (LED_DM_DIG_HIZ << (6 * 3))); /* High Impedance Digital */

    /* 6 is a pin number, 3 and 4 are bitfield widths */

    CySysClkWriteHfclkDirect(CY_SYS_CLK_HFCLK_EXTCLK);

    for(;;)

    {

        LED_Write(0);

        CyDelay(500);

        LED_Write(1);

        CyDelay(500);

    }

}

I have attached the sample project below.

Best Regards

Ekta

View solution in original post

0 Likes
MaMi_1205306
Honored Contributor

Ekta-san,

Thank you for your response.

Added changes to register settings suggested by you.
Then, it was confirmed that the clock switched normally.


I think that the compile contents set to ECO are different for each device or maybe the version of the boot component.
We hope there is an application note.

Regards,

0 Likes
Ekta
Moderator
Moderator

Hello Masashi -San,

This issue will be fixed in the next release of PSoC Creator.

Best Regards

Ekta

0 Likes
MaMi_1205306
Honored Contributor

Ekta-san,

I understood that it will improve in the next version of PSoC Creator.
I appreciate your support.

Regards,

0 Likes