Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
RyYo_1406951
Level 5
Level 5
100 replies posted 50 replies posted 25 replies posted

Below, the same sentences are written in English and Japanese.

Below is the continuation of the thread.
https://community.cypress.com/thread/46072

・Engilsh
The only way to decide on the "resolution bit" is to connect a sensor to PSoC and select the optimum value?

・日本語(japanese)
"Resolution bit"を決定する為には、実機で動作し、最適値を求めるしかないでしょうか?

Regards

0 Likes
1 Solution
Takashi_M
Moderator
Moderator
Moderator
1000 replies posted 500 solutions authored 750 replies posted

Yes, you have to choose the appropriate "resolution" with the complete hardware.

The "resolution" is the one of tuning factor, so it can not be estimate earlier.

View solution in original post

2 Replies
Takashi_M
Moderator
Moderator
Moderator
1000 replies posted 500 solutions authored 750 replies posted

Yes, you have to choose the appropriate "resolution" with the complete hardware.

The "resolution" is the one of tuning factor, so it can not be estimate earlier.

Thank you for your answer.

0 Likes