Hello
I will use IAR Workbench as my IDE and compiler.
Chip is CY8C4147AZI-S455.
I have TTBridge(CY3295) and miniprog3.
but there is no selective option for cypress tool.
can I use this cypress tool for debugger?
If it is possible, How can I set my environment?
Regards,
Sunghun noh
Solved! Go to Solution.
Hello
We regret to say that presently it is not possible to use Cypress programmers like Miniprog 3/Miniprog 4/Kitprog with IAR Embedded workbench. You need to use either J-Link/ I-Jet to program the devices through IAR.
Cypress is actively working to add support for PSoC 4 in Modus Toolbox though PDL in the near future. Then you can use cypress programmers to program your applications over Windows, Linux and Mac.
Thanks
Ganesh
Hello
We regret to say that presently it is not possible to use Cypress programmers like Miniprog 3/Miniprog 4/Kitprog with IAR Embedded workbench. You need to use either J-Link/ I-Jet to program the devices through IAR.
Cypress is actively working to add support for PSoC 4 in Modus Toolbox though PDL in the near future. Then you can use cypress programmers to program your applications over Windows, Linux and Mac.
Thanks
Ganesh
I got it.
I will try using Jlink.
Thanks Ganesh.