cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

suno_285741
New Contributor II

Hello

I will use IAR Workbench as my IDE and compiler.

Chip is CY8C4147AZI-S455.

I have TTBridge(CY3295) and miniprog3.

but there is no selective option for cypress tool.

can I use this cypress tool for debugger?

If it is possible, How can I set my environment?

pastedImage_0.png

Regards,

Sunghun noh

0 Likes
1 Solution
VenkataD_41
Moderator
Moderator

Hello

We regret to say that presently it is not possible to use Cypress programmers like Miniprog 3/Miniprog 4/Kitprog with IAR Embedded workbench. You need to use either J-Link/ I-Jet to program the devices through IAR.

Cypress is actively working to add support for PSoC 4 in Modus Toolbox though PDL in the near future. Then you can use cypress programmers to program your applications over Windows, Linux and Mac.

Thanks

Ganesh

View solution in original post

2 Replies
VenkataD_41
Moderator
Moderator

Hello

We regret to say that presently it is not possible to use Cypress programmers like Miniprog 3/Miniprog 4/Kitprog with IAR Embedded workbench. You need to use either J-Link/ I-Jet to program the devices through IAR.

Cypress is actively working to add support for PSoC 4 in Modus Toolbox though PDL in the near future. Then you can use cypress programmers to program your applications over Windows, Linux and Mac.

Thanks

Ganesh

suno_285741
New Contributor II

I got it.

I will try using Jlink.

Thanks Ganesh.

0 Likes