- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have Psoc cy8ckit-042 connected with 2 SCB Uart ports. One to the PC and the other to a SIM7600A GSM module. Programming and debug for the cy8ckit is via the onboard usb port.
P4.0 and P4.1 connected to the SIM7600. P0.4 and P0.5 connected to the PC via a Silicon Labs CP210x USB to UART Bridge.
I have tried multiple communication programs but Putty works as well as others. I can enter all the AT commands to the sim 7600 from putty and they work fine. But I cannot get the psoc to send commands to the sim 7600 without losing quite a bit of the message. I have tried turning the echo on and off. No difference. I’ve tried delays, no difference.
I’m using an interrupt to initiate a simple AT command to the SIM7600. When the interrupt is initiated, It prints to the PC uart (Putty) and it works fine, but I print to the sim7600 and it loses many of the characters.
A similar setup works fine using Arduino. I have tried many scenarios to get this to work on the PSOC but it does not cooperate.
I am using an interrupt handler for each UART for receiving. The basic program came from your CE224406_PSoC4_UART.pdf.
I have attached an archive of the project. You may ignore the functions that are not being used.
Any suggestions?
Thank-you
Solved! Go to Solution.
- Labels:
-
ispn:39611:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank-you. I downloaded "two_uart_200425", set the pins, adjusted the board
rate and it runs perfectly.
The project is similar to mine except it collects an entire line where I
was responding to each character. Should be interesting.
I will add an interrupt handler to respond with a message to the GSM module
based on a pin going high.
I will let you know how it works.
Thanks again
Doug
On Thu, Dec 31, 2020 at 8:56 PM BiBi_1928986 <community-manager@cypress.com>
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello.
You might want to read this discussion. Similar project, 2 UARTs, CY8C4245 on KIT-049 (same PSoC as KIT-042), GSM module.
UART RX INTERRUPT PROGRAM FOR CY8CKIT 49
It starts off to get UARTs working using same app note CE224406, eventually talks with GSM module.
Good luck with our project.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank-you. I downloaded "two_uart_200425", set the pins, adjusted the board
rate and it runs perfectly.
The project is similar to mine except it collects an entire line where I
was responding to each character. Should be interesting.
I will add an interrupt handler to respond with a message to the GSM module
based on a pin going high.
I will let you know how it works.
Thanks again
Doug
On Thu, Dec 31, 2020 at 8:56 PM BiBi_1928986 <community-manager@cypress.com>
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Doug.
Great news! A good way to start off the new year.
Bill
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I have 2 UARTs working. I can type a simple command like AT or ATE1 on the pc, it goes to the psoc via uartCMD which sends it to the GSM modem via uartGSM. I get a response "OK" from the UART_GSM which shows up on the PC via the UART_CMD. I can even send a set of commands which result in a text message being sent to my phone. Therefore the GSM is working, the 2 uarts are working.