- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello everyone,
I am facing this issue with the CapSense tuner that I cannot seem to troubleshoot.
I am using CYBLE-222005-EVAL Connected to CY8CKIT-042-BLE Pioneer dev board and MiniProg 3
I have a simple capacitive sensor connected to the dev board. I am trying to use the Capsense Tuner to tune the sensor output
I am using the example from PSoC creator "PSoC4 CapSense Low Power-One Button"
Once I try to establish the connection to the tuner, I get this error "There was an error reading data from the device "
s
I added screenshots below of the configuration parameters for both the Tuner and EZI2C
I would like to ask if someone faced this issue before, and how to resolve it,
Your help is very much appreciated.
Thanks in advance
Solved! Go to Solution.
- Labels:
-
PSoC 4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @ThWe_4461836 , This issue typically happens when there is an issue in the I2C settings or the I2C connections. Miniprog supports I2C connections in the 5 pin connector and not in the 10 pin connector. From what I see, you have used the 10 pin programming connector between the miniprog and the module. For the I2C connection, you need to make the following connections between the 5 pin connector and the pioneer kit base board.
I2C pins are the SDAT and SCLK. Connect the ground together and Vtarg if required.
Bragadeesh