Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
user_4621631
Level 1
Level 1
First like given

Hello!

On peripheral device side I'm trying to acquire the address of the connected central device when it gets connected.

Central device MAC is actually 00A050DC77C7, but when the connection is established I get an event like:

@E,0035,C,C=04,A=804929199580,T=00,I=0006,L=0000,O=0064,B=00

I tried with multiple different modules as central devices and all of them give me the address 804929199580.

I'm using a simple configuration on the central side:

.CYSPPSP,E=2,R=11223344,L=11223344,M=FFFFFFFF,G=1,S=0

SAP,L=0

SSP,F=0

/SCFG

/RBT

and on the peripheral side:

.CYSPPSP,E=2,R=11223344,L=11223344,M=FFFFFFFF,G=0,S=0

SAP,L=0

SSP,F=0

/SCFG

/RBT

On the central device I tried running GBA command, but it always returns actual MAC address:

@R,0018,GBA,0000,A=00A050DC77C7

I noticed the occurrence of this address in some other topics (e.g https://community.cypress.com/thread/45727?start=0&tstart=0), but haven't figured out what it actually means.

How should I reorganise the program to get the actual connected device's mac address?

0 Likes
1 Solution
Yugandhar
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 1000 replies posted

Hello,

At the central side, please make sure that before initiating a connection with the peripheral device, the module must be in a disconnected state (not advertising, scanning, connecting, or connected). Before doing the connection please set the /DIS, /SX, /AX commands as shown in below.

*********************************************

/dis

@R,000A,/DIS,0502

/ax

@R,0009,/AX,0000

@E,000E,ASC,S=00,R=00

/sx

@R,0009,/SX,0107

/c, A=00a050708225

@R,000D,/C,0000,C=00

@E,0035,C,C=04,A=00A050708225,T=00,I=0006,L=0000,O=0064,B=00

*********************************************

Thanks,

P Yugandhar.

View solution in original post

0 Likes
1 Reply
Yugandhar
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 1000 replies posted

Hello,

At the central side, please make sure that before initiating a connection with the peripheral device, the module must be in a disconnected state (not advertising, scanning, connecting, or connected). Before doing the connection please set the /DIS, /SX, /AX commands as shown in below.

*********************************************

/dis

@R,000A,/DIS,0502

/ax

@R,0009,/AX,0000

@E,000E,ASC,S=00,R=00

/sx

@R,0009,/SX,0107

/c, A=00a050708225

@R,000D,/C,0000,C=00

@E,0035,C,C=04,A=00A050708225,T=00,I=0006,L=0000,O=0064,B=00

*********************************************

Thanks,

P Yugandhar.

0 Likes