Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

PSoC™ 4 Forum Discussions

Anonymous
Not applicable

PSoC 4 BLE is a single-chip SoC that integrates the following:

   

 

   

- ARM Cortex-M0 CPU up to 48 MHz

   

- 256/32Kb, 128/16Kb Flash/SRAM (128Kb sampling now, 256Kb coming soon)

   

- 2.4 GHz Bluetooth Low Energy Radio with Integrated Balun

   

- 4 x Opamps (operational in Deep-Sleep Mode)

   

- 2 x Comparators (operational in Deep-Sleep Mode)

   

- 1 x SAR ADC 12bit, 1-Msps with 8-ch Sequencer

   

- 1 x CapSense CSD block for touch-sensing

   

- 4 x TCPWM (Timer/Counter/PWM) blocks

   

- 2 x SCB (Serial Communication UART/SPI/I2C) block

   

- 4 x UDB (Universal Digital Blocks, PLD-based programmable logic) blocks

   

- 1 x Segment LCD block

   

- 36 GPIO

   

- Five low-power modes (Active, Sleep, Deep-Sleep, Hibernate, Stop Modes)

   

 

   

 

   

 

   

A block diagram of the device can be see here: PSoC 4 BLE Block Diagram

   

 

   

The device datasheet (prelim) is available here: PSoC 4 BLE Datasheet

0 Likes
1 Solution
Bob_Marlowe
Level 10
First like given 50 questions asked 10 questions asked
Level 10

The Cypress programmer will be updated when new chips are to come. Even the MiniProg is able to receive a new firmware (see item in Programmer) so that you do not have to purchase new equipment.

   

 

   

Bob

View solution in original post

0 Likes
4 Replies
AsRa_264661
Level 4
50 replies posted 25 replies posted 10 likes received
Level 4

Hi Gagan,

   

Very great!  welcomes to PSOC 4 BLE,

   

The question here is , MiniProg3 has the capable to program this BLE chip?

   

 

   

Thanks,

   

Ashok r

0 Likes
Anonymous
Not applicable

 There are 2 easy ways to program PSoC 4 BLE devices:

   

 

   

1. Use the BLE Pioneer Kit, which has an on-board 'KitProg' Programmer and Debugger

   

or 

   

2. Use the MiniProg3 with the latest version of PSoC Programmer which supports the new PSoC 4 BLE devices

0 Likes
AsRa_264661
Level 4
50 replies posted 25 replies posted 10 likes received
Level 4

Hi Gagan,

   

Recently i purchased MiniProg3 so will it work or not?

   

any how the new Psoc Creator has released right so it should work? correct?

   

 

   

Thanks,

   

Ashok r

0 Likes
Bob_Marlowe
Level 10
First like given 50 questions asked 10 questions asked
Level 10

The Cypress programmer will be updated when new chips are to come. Even the MiniProg is able to receive a new firmware (see item in Programmer) so that you do not have to purchase new equipment.

   

 

   

Bob

0 Likes