I am developing a current mirror circuit using the PSOC4BLE IDAC as the current source as shown in the figure. If I am supplying 100micro Ampere current, I am getting 2260micro Ampere current.
Please find the circuit in the attached image.
Can someone suggest the solution?
Solved! Go to Solution.
BhSr,
Please check these threads
Increasing Voltage Compliance with iDAC and Current Mirror
/odissey1
Hi,
Could you please check the compliance votage parameter of the IDAC. Does the voltage come within the operating voltage of the IDAC in your use-case ?
Best Regards,
Vasanth
BhSr,
Hopefully I understood your diagram correctly. I have a couple of issues with your circuit intention.
First Issue: You are trying to source the IDAC8 current from VSS (GND). This is not correct.
The IDACs on the PSoC can only sink current into GND or source current from VSSA.
Second issue: Even if you were sinking current into GND through the IDAC, you have the bias voltage at -5V. No PSoC input or output is supposed to be less than VSS-0.5V.
BhSr,
Please check these threads
Increasing Voltage Compliance with iDAC and Current Mirror
/odissey1