Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
ToVa_285016
Level 5
Level 5
100 replies posted 50 replies posted 50 questions asked

Hi,

   

I am very interested in the mesh flood example (Day 49 in the 100 projects/100 days) for a project I am working on, indeed it is almost  exactly what I need.

   

What I want to do is make one of the PSOC BLE's a controller who's only role is to send our the RGB data at the push of a button.  I am looking at modifying the existing mesh flood example code, and hopefully simplifying it greatly.  I am new to BLE, and it is wildly more complicated than the BT serial links I am used to dealing with.  

   

Where do I start with this?  Do I need to modify the custom profile?  Are any of the examples similar to what I am trying to do?  

   

I saw Cypress had a demo at CES that was very similar to what I am looking for with a proximity sensor controlling light bulbs that were in a mesh - does this code exist somewhere?

   

Thank you,
Tom

0 Likes
1 Solution
Anonymous
Not applicable

Hi Tom,

   

Yes, using custom profile would be good for your application. You can refer to this Application Note:

   

AN91162 - Creating a BLE Custom Profile (http://www.cypress.com/documentation/application-notes/an91162-creating-ble-custom-profile)

   

The demo shown at CES was based on Smart Mesh which is a new spec by Bluetooth SIG. This is still under development.

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Hi Tom,

   

Yes, using custom profile would be good for your application. You can refer to this Application Note:

   

AN91162 - Creating a BLE Custom Profile (http://www.cypress.com/documentation/application-notes/an91162-creating-ble-custom-profile)

   

The demo shown at CES was based on Smart Mesh which is a new spec by Bluetooth SIG. This is still under development.

0 Likes