Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
AdamsChengTW
Level 3
Level 3
10 sign-ins 5 sign-ins 10 questions asked

I have a SPI slave mode problem with interrupt mode.

When I use polling communication is normal. I can receive SPI Master  frame and response slave frame data.

But, I try interrupt mode. it Will be stuck in the interrupt sub function.

The program strucks on this line in debug mode. -->  while (PACKET_SIZE != SPI_SpiUartGetRxBufferSize()) 

The blow is my PSoc creator setting and program screenshot.

spi4.jpg

spi5.jpg

my program screenshot

1. ISR function

spi7.jpg

2. Enable interrupt

spi8.jpg

3. ISR function

spi6.jpg

0 Likes
1 Solution
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

I'm sorry I miss-read PSoC 4100 SPI Slave as PSoC 4100S Plus. (It's Monday)

Anyway, could you try to configure your SPI as

003-4125-spi.JPG

moto

P.S. Attached is my test sample for CY8C4125LQI-483.

As we have only 2 SCBs, I deleted SPIM, which I used to generate test data.

The project is compile-able, but as I don't have board with this device, I have not tested it.

View solution in original post

4 Replies
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

I think that the interrupt of SPI happens each byte.

So I would do instead of gathering the whole packet,

pick up each byte in the ISR and when the buffer index reaches to PACKET_SIZE set the flag.

==================

CY_ISR(SPI_ISR)

{

    if ((SPI_GetRxInterruptSourceMasked() & SPI_INTR_RX_NOT_EMPTY) != 0) {

       

        if (0u != SPI_SpiUartGetRxBufferSize()) {

            MasterFrame[rx_buf_index] = (uint8_t) SPI_SpiUartReadRxData() ;

            rx_buf_index++ ;

        }

       

        /* Clear interrupt flag */

        SPI_ClearRxInterruptSource(SPI_INTR_RX_NOT_EMPTY) ;

       

        if (rx_buf_index == PACKET_SIZE) {

            rx_buf_index = 0 ;

            spi_flag = AS_TRUE ;

        }

    }  

==================

Following is my trial with CY8CKIT-149

schematic

001-schematic.JPG

pins

Note: I connected following 4 pairs using jumper wires

SPI:miso_s - SPIM:miso_m

SPI:mosi_s - SPIM:mosi_m

SPI:sclk_s   - SPIM:sclk_m

SPI:ss_s  - SPIM:ss0_m

002-pins.JPG

main.c

=================

#include "project.h"

#include "stdio.h"

#define AS_TRUE    (1u)

#define AS_FALUSE  (0u)

#define PACKET_SIZE 10

volatile int spi_flag = 0 ;

volatile int rx_buf_index = 0 ;

uint8_t MasterFrame[PACKET_SIZE] = { 0u } ;

#if 0

CY_ISR(SPI_ISR)

{

    uint8_t FrameIndex = 0 ;

   

    if ((SPI_GetRxInterruptSourceMasked() & SPI_INTR_RX_NOT_EMPTY) != 0) {

        /* Waits for the end of the data transfer */

        while(PACKET_SIZE != SPI_SpiUartGetRxBufferSize()) {

            ;

        }

       

        while(0u != SPI_SpiUartGetRxBufferSize()) {

            MasterFrame[FrameIndex] = (uint8_t) SPI_SpiUartReadRxData() ;

            FrameIndex++ ;

        }

       

        /* Clear rx buffer */

        SPI_SpiUartClearRxBuffer() ;

       

        /* Clear interrupt flag */

        SPI_ClearRxInterruptSource(SPI_INTR_RX_NOT_EMPTY) ;

       

        spi_flag = AS_TRUE ;

    }  

}

#else

CY_ISR(SPI_ISR)

{

    if ((SPI_GetRxInterruptSourceMasked() & SPI_INTR_RX_NOT_EMPTY) != 0) {

       

        if (0u != SPI_SpiUartGetRxBufferSize()) {

            MasterFrame[rx_buf_index] = (uint8_t) SPI_SpiUartReadRxData() ;

            rx_buf_index++ ;

        }

       

        /* Clear interrupt flag */

        SPI_ClearRxInterruptSource(SPI_INTR_RX_NOT_EMPTY) ;

       

        if (rx_buf_index == PACKET_SIZE) {

            rx_buf_index = 0 ;

            spi_flag = AS_TRUE ;

        }

    }  

}   

#endif

#define STR_LEN 64

char    str[STR_LEN+1] ;

void    print(char *str)

{

    UART_UartPutString(str) ;

}

void   printc(char c)

{

    UART_UartPutChar(c) ;

}

void cls(void)

{

    print("\033c") ; /* reset */

    CyDelay(20) ;

    print("\033[2J") ; /* clear screen */

    CyDelay(20) ;

}

void splash(void)

{

    cls() ;

    print("PSoC 4100S Plus SPI test") ;

    snprintf(str, STR_LEN, "(%s %s)\n", __DATE__, __TIME__) ;

    print(str) ;

}

void init_hardware(void)

{

    CyGlobalIntEnable; /* Enable global interrupts. */

    UART_Start() ;

    splash() ;

   

    SPIM_Start() ;

   

    isr_1_ClearPending() ;

    isr_1_StartEx(SPI_ISR) ;

    SPI_Start() ;

}

void clear_MasterFrame(void)

{

    int i = 0 ;

    for (i = 0 ; i < PACKET_SIZE ; i++ ) {

        MasterFrame = 0 ;

    }

}

void send_packet(void)

{

    uint8_t tx_buffer[PACKET_SIZE] = { '0', '1', '2', '3', '4', '5', '6', '7', '8', '9' } ;

    SPIM_SpiUartClearTxBuffer() ;

    SPIM_SpiUartPutArray(tx_buffer, PACKET_SIZE) ;

}

void dump_rx_buffer(void)

{

    int i = 0 ;

    for (i = 0 ; i < PACKET_SIZE ; i++ ) {

        printc(MasterFrame) ;

    }

    print("\n\r") ;

}

int main(void)

{  

    init_hardware() ;

    send_packet() ;

   

    for(;;) {

        if (spi_flag) {

            spi_flag = 0 ;

            dump_rx_buffer() ;

            clear_MasterFrame() ;

            CyDelay(1000) ;

           send_packet() ;

        }

    }

}

=================

Tera Term log

000-TeraTerm-log.JPG

moto

Hi Moto,

My mcu type is CY8C4125LQI-483 and PSoc creator 4.2

I can not find SPI interrupt In the schematic.

0 Likes
lock attach
Attachments are accessible only for community members.
MotooTanaka
Level 9
Level 9
Distributor - Marubun (Japan)
First comment on blog Beta tester First comment on KBA

Hi,

I'm sorry I miss-read PSoC 4100 SPI Slave as PSoC 4100S Plus. (It's Monday)

Anyway, could you try to configure your SPI as

003-4125-spi.JPG

moto

P.S. Attached is my test sample for CY8C4125LQI-483.

As we have only 2 SCBs, I deleted SPIM, which I used to generate test data.

The project is compile-able, but as I don't have board with this device, I have not tested it.

Dear Moto,

I try your sample it working in interrupt mode.

Thank you for your help.