- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello All,
Quick question that I am pretty certain I know the answer but I don't see it spelled out clearly in the RTC_P4_v1_20.pdf document.
When in 24 hour clock mode does the AM_PM flag get set when the time is between 12:00 & 23:59:59?
I am pretty certain the answer is "no" but I also don't see it clearly defined in the datasheet. So I thought I would check with the community.
Thanks,
Dave
Solved! Go to Solution.
- Labels:
-
PSoC 4 Architecture
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I've just checked with RTC_P4_V1_10 in PSoC Creator v4.2 with a project for CY8C4247AZI-M485 (CY8CKIT-044)
If with "AM_PM flag" you meant is the bit 22 of dateTime->time which is acquired from
RTC_UnixToDateTime() function, I think that you are correct.
In RTC_UnixToDateTime() the variable tmpAmPmState is initialized as 0u. (line 1377 of RTC.c)
And only when timeFormat is not RTC_24_HOURS_FORMAT (line 1426 of RTC.c)
tmpAmPmState has chance to be assigned RTC_PM (line 1430 of RTC.c).
Then for the dataTime->time, RTC_ConstructTime is called with the 2nd argument "tmpAmPmState",
which is always 0 when date format is RTC_24_HOURS_FORMAT ,
so there will not be a chance to get that bit be set in RTC_ConstructTime(). (line 1450 of RTC.c)
moto